+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
A resistance thermometer (Resistance Temperature Detector, RTD) is a precision temperature sensor whose operating principle is based on the phenomenon of change in the electrical resistance of a metal as a function of temperature. As the temperature increases, the resistance of the conductor increases in a predictable and measurable manner, allowing the temperature value to be accurately determined by measuring the electrical resistance of the sensing element.
The active element of a resistance thermometer is usually a thin wire or layer of metal with well-known temperature properties, most commonly platinum, due to its chemical stability, resistance to oxidation and the linear nature of resistance changes. Platinum sensors, such as PT100 or PT1000, denote 100 and 1000 ohms of resistance at 0 °C, respectively, and are commonly used in industrial, scientific and laboratory measurements.
RTDs are characterised by high accuracy, repeatability and long-term measurement stability. Their temperature response is well described by a non-linear function that can be converted to a linear approximation or described by the Callendar-Van Dusen equations. Others circuit configurations - two-, three- or four-wire - are used to measure resistance in RTD thermometers, aiming to eliminate errors due to the resistance of the connecting cables.
Resistance thermometers are used in industrial automation systems, process monitoring, HVAC systems, power generation, aerospace and medical and food applications. Their operation can be integrated with analogue and digital transmitters, enabling the processing of the resistance signal into voltage, current or digital signals according to the requirements of the control system and Data Acquisition Systems.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.