+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Thermocouple is a temperature sensor that uses the Seebeck effect to precisely measure the temperature difference between two connected conductors made of Others metals or Feet. Its operation is based on the generation of a thermoelectric voltage as a result of the temperature gradient between the reference point and the measuring junction, allowing the temperature difference to be converted into an electrical signal proportional to the measured temperature value.
The basic structure of a thermocouple consists of two metallic conductors connected at one end, where thermal energy is converted to electrical potential. Reading the voltage generated at the open end of the system requires the use of reference temperature compensation, which is realised by compensating circuits or digital corrections based on additional semiconductor sensors. The voltage-thermal characteristics depend on the material composition of the conductors used, which determines the operating range and measurement accuracy.
Due to the specific properties of the metals used in the construction of thermocouples, a distinction is made between standard types such as K (nickel-chromium/nickel-alumel), J (iron-constantan), T (copper-constantan) or S and R (platinum-rhodium), which differ in temperature range, stability and resistance to chemical environments. High-temperature thermocouples are used in metallurgy, power generation and materials engineering, while low-temperature models are used in cryogenic systems, research laboratories and applications HVAC.
Interfacing thermocouples with measurement systems requires high-resolution analogue-to-digital converters and cold junction compensation systems to minimise measurement errors due to ambient temperature effects. Microprocessor chips used in modern Data Acquisition Systems implement algorithms to correct non-linearity in thermocouple characteristics, allowing accurate temperature readings over a wide measurement range.
The ruggedness of thermocouples is due to the use of specialised protective sheaths made of ceramic, stainless steel or oxidation-resistant alloys, enabling their use in aggressive chemical environments, high pressures and extreme temperature conditions. Their design can include Mineral Insulated (MI) Guards, increasing mechanical resistance and reducing the response time to temperature changes, which is crucial in dynamic processes.
Thermocouples are used in a wide range of applications, including industrial process control, internal combustion engine diagnostics, power system monitoring and scientific research requiring high measurement precision. The integration of thermocouples with IoT systems and telemetry networks enables real-time remote temperature monitoring and the implementation of predictive maintenance algorithms, which increases the reliability and operational efficiency of industrial and research systems.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.