+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Ultrasound - definition

Ultrasound are mechanical waves propagating in elastic media, whose frequency exceeds the upper limit of hearing of the human ear, which is approximately 20 kHz. Due to their nature, ultrasound is not perceived by humans as sound, but exhibits important physical and technological properties that enable its wide application in technology, medicine and science.

Ultrasound waves are longitudinal and transverse in nature and their propagation depends on the properties of the material through which they propagate - including density, elasticity and internal structure. The frequency of ultrasound determines its ability to penetrate materials and its resolution in diagnosis and detection. In higher frequency bands, imaging precision increases but penetration depth decreases.

In technology, ultrasound is usually generated using piezoelectric transducers or magnetostrictive transducers, which convert electrical energy into high-frequency mechanical vibrations. These vibrations can be used to probe the interior of objects, detect defects, measure distances, locate obstacles or image the inside of the human body. In industrial applications, ultrasound plays a key role in cleaning, welding, emulsifying or accelerating chemical reactions, thanks to its ability to generate cavitation and local pressure changes.

From the point of view of technical acoustics and Automation, ultrasound is used as an information carrier in non-contact Measurement Sensors, positioning systems, presence detection and echolocation-based control systems. Their use requires consideration of parameters such as wavelength, acoustic impedance, attenuation in the medium and reflection at phase boundaries, which affect the accuracy and efficiency of ultrasonic systems.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO