+1 500 000 products in offer
6000 packages per day
+300 000 clients from 150 countries
WAN (Wide Area Network) is a wide-area computer networka enabling the exchange of data between devices and systems located at great geographical distances - from tens to thousands of kilometres. A WAN is an infrastructure connecting local area networks LAN (Local Area Network) and other network segments into a coherent whole, operating on a global or interregional level. Its primary purpose is to provide communication and access to information resources in distributed locations, regardless of physical boundaries.
WANs are based on a variety of transmission technologies, including fibre-optic connections, satellite links, mobile networks and Internet protocols such as MPLS, Frame Relay or classic IP. Depending on the users' needs and available resources, the WAN can be built using leased transmission lines, VPN tunnels, point-to-point connections or public Internet infrastructure. Its topology and level of management depend on the scale and complexity of the deployment.
At the functional layer, the WAN operates at several levels of the OSI model, using devices such as routers, Layer 3 switches, VPN hubs and network security systems. Key design aspects include bandwidth, transmission delay, redundancy, reliability and security of transmitted data. Today's WANs are often managed using advanced software-defined technologies such as SD-WAN (Software-Defined WAN), which enable dynamic traffic control and real-time connection optimisation.
The WAN plays a fundamental role in the operation of distributed organisations, cloud service providers, government institutions and global communication systems. Its architecture enables location-independent access to data and services, supporting remote working, multimedia transfer, synchronisation of databases and the implementation of advanced network services.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.