+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Moisture meter - definition

Moisture meter is a measuring instrument used to determine the water vapour content of gases, most often in atmospheric air, or in solid materials and liquids. Its primary task is to determine the relative humidity, absolute humidity or dew point, depending on the specific application. Relative humidity is the ratio of the current amount of water vapour to the maximum amount that the air can hold at a given temperature, expressed as a percentage.

Others use different principles of operation depending on the application and measurement requirements: psychrometric, condensation, capacitive, resistive or optoelectronic methods. Psychrometric moisture meters are based on measuring the temperature difference between a dry and a wet thermometer, while capacitive instruments measure the dielectric changes of a moisture-responsive material. Modern Humidity Sensors often integrate humidity measurements with temperature measurements, allowing the calculation of additional parameters such as point or absolute humidity.

In engineering, moisture meters are indispensable tools in air conditioning, food and beverage, pharmaceutical, materials and construction industries, where moisture control is crucial to maintain product quality, optimise processes and maintain appropriate environmental conditions. In Automation systems, humidity meters are elements of microclimate monitoring and control systems, ensuring stability of environmental parameters in clean rooms, server rooms or warehouses for moisture-sensitive raw materials. The design of modern hygrometers often includes communication interfaces (e.g. Modbus, I²C, 4-20 mA), enabling their integration with SCADA systems and Internet of Things (IoT) solutions.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO