+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Overcurrent circuit breaker (circuit breaker) - definition

Circuit Breakers is a mechanical protective switch designed to automatically interrupt the flow of electric current in a circuit when a certain current value is exceeded. Its function is to protect the electrical installation, consumers and users from the effects of overloads and short circuits that can lead to overheating of the Cables, damage to the equipment or fire. The overcurrent circuit breaker has a protective function comparable to a fuse, but has the ability to be repeatedly switched on after tripping, making it easier to operate and service.

The essential design elements of an overcurrent circuit breaker are the overload and short-circuit detection mechanisms. The overload action is realised by means of a thermal trip, usually in the form of a bimetal that bends when the temperature rises, triggering the disconnection mechanism. Short-circuit is detected by an electromagnetic trigger - a coil that generates a force upon a sudden increase in current, allowing the contacts to open immediately. In both cases, the opening of the current path interrupts the flow of energy to the protected section of the installation.

Circuit Breakers are classified according to the time-current characteristic, which defines the response time of the device depending on the level of current. Characteristics B, C and D are the most commonly used, differing in their sensitivity to current pulses and their suitability for different types of consumer. Modern circuit breakers can also integrate additional functions such as residual current protection, remote control capability or communication in building automation systems.

In installation practice, the overcurrent circuit breaker is mounted on a DIN rail in switchgear and is an essential component of the short-circuit and overload protection system. The selection of a suitable model requires consideration of the current rating, protection characteristics and short-circuit parameters of the network. The operation of the circuit breaker should comply with the applicable standards, including IEC 60898 or EN 60898.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO