+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Electroacoustic amplifier - definition

An electroacoustic amplifier is an electronic device designed to increase the amplitude of acoustic signals converted to electrical form for effective reproduction by speakers, headphones or other electroacoustic transducers. It is a key component of the audio path, connecting the sound source - such as a microphone, musical instrument, player - to the end devices used to emit sound. Its task is to ensure the appropriate level of power and quality of the processed signal while maintaining the lowest possible distortion.

From a technical point of view, an electroacoustic amplifier performs the function of amplifying a voltage or current signal without changing its shape and frequency characteristics. It usually consists of several stages: a preamplifier, a tone corrector, a power stage and protection circuits. Others can operate in different amplification classes (e.g. A, B, AB, D), which determine power efficiency, linearity and thermal characteristics. Modern designs often use pulse amplifiers (class D), characterised by high efficiency and compact size.

Electroacoustic amplifiers are divided into analogue and digital, with the latter using digital domain signal processing (DSP), which enables advanced equalization, filtering and dynamic sound processing algorithms. These devices can be stand-alone components of sound systems or part of integrated audio systems in consumer, professional and industrial equipment.

Parameters describing the quality of an amplifier include frequency response, non-linear distortion coefficient (THD), signal-to-noise ratio (SNR) and output power. Their selection and configuration depend on the application requirements, the type of transducers and the acoustic characteristics of the environment in which the amplifier is used. In sound engineering and acoustics, the electroacoustic amplifier plays a fundamental role in achieving the desired sound, dynamics and spatiality of the audio signal.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO