+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Operational amplifiers is a universal, high-power electronic component, usually implemented as an integrated circuit, designed to amplify the voltage difference between two inputs: non-inverting and inverting. Its operation is based on the principle of feedback, which allows precise control of the gain and the shape of the processed signal. Thanks to its versatility, the operational amplifier is a basic functional block in analogue electronic circuits, such as filters, integrators, differentiators, comparators, amplifiers or analogue-to-digital converters-digital converters.
The ideal operational amplifier is characterised by infinite open-circuit voltage gain, infinite input impedance and zero output impedance, which means, that it does not load the signal source and can drive any load without signal loss. In practice, these parameters are physically limited, but modern designs provide very high performance in a wide range of applications.
Operational amplifiers are designed to operate in linear and non-linear configurations. In linear configurations, they implement.inter alia. precise amplification of analogue signals, voltage summing, filtering and correction. In non-linear applications, they can act as threshold detectors, switches or waveform generators. Wide frequency range, low noise, fast impulse response and the ability to work with very small signals make them indispensable in measurement systems, data acquisition and audio devices.
Structurally, an operational amplifier contains internal input stages for, amplifying and output stages, usually based on Bipolar transistors or MOSFETs-ach, and its operation depends on external passive components, which define the circuit function. Standard models, such as the LM741, TL081 or modern op-rail type op amps-are-rail, are widely used in education, research and electronics industry.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.