+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Guide to Coaxial Cables – Structure, Operating Principle and Basic Concepts

Date of publication: 03-02-2026 🕒 7 min read

Coaxial cables play a key role in today's telecommunications world, providing reliable signal transmission in various applications. Have you ever wondered how they work and why they are so important in our daily lives? In this article, we will take a closer look at coaxial cables, their construction, operating principle, and significance in telecommunications.

A coaxial cable is a type of electrical cable consisting of a central core surrounded by an insulating layer and a shield. Its history dates back to 1880 when it was invented by Oliver Heaviside. Since then, coaxial cables have revolutionized the way we transmit information, enabling the development of telephony, cable television, and many other technologies.

Key Information in Brief

Coaxial cables, also known as coax cables, are an essential component of modern telecommunications infrastructure, providing reliable signal transmission in various applications. Their construction, consisting of a central copper core, insulation, shielding, and an outer jacket, allows effective protection of the signal from electromagnetic interference. These cables are used in telecommunications, cable TV, as well as in audio-video systems and surveillance.

Key technical parameters such as characteristic impedance (50Ω and 75Ω), signal attenuation, and shielding effectiveness are essential for selecting the appropriate cable depending on the specific project requirements. Despite some disadvantages, such as installation challenges or sensitivity to environmental conditions, coaxial cables offer many advantages, including resistance to mechanical damage and versatile applications.

Looking ahead, coaxial cables will continue to play an important role, especially in hybrid fiber-coaxial networks and in the context of modern technologies like 5G. By understanding their construction, operation, and applications, both hobbyists and professionals can effectively use coaxial cables in their projects, opening new possibilities for innovation in telecommunications. We encourage further exploration of this versatile solution.

How a Coaxial Cable Is Constructed

A coaxial cable, also known as a coax cable, consists of four basic layers that work together to provide effective signal transmission. The central copper wire is the main conductor that carries electrical signals. Surrounding it is the internal insulation (dielectric), which prevents short circuits and minimizes signal loss. Next is the shield (braid), which acts as protection against electromagnetic interference, shielding the signal from external influences. The entire structure is enclosed by the outer insulation (jacket), which protects the cable from mechanical damage and environmental impact.

In practice, the signal propagates as an electromagnetic wave guided by the cable’s structure. The signal is transmitted through the inner conductor, while the outer shield serves as the return conductor. Signal quality is closely related to the braid density — the denser and more uniform the shield, the better the signal is protected from interference and loss. During transmission, the signal generates an electromagnetic field between the internal conductor and the shield, which helps maintain signal stability and purity. Understanding this construction and operating principle is key to effectively using coaxial cables in practical applications, both domestic and professional.

Coaxial connection cables

What Are the Applications of Coaxial Cables

Coaxial cables have many practical applications that make them an indispensable part of today’s telecommunications infrastructure. Primarily, they transmit signals in telecommunications, where their ability to minimize electromagnetic interference makes them the ideal medium for transmitting radio and digital signals. Thanks to a wide bandwidth, coaxial cables are also used in antenna installations and cable television, delivering signals to homes and businesses in hybrid fiber-coaxial (HFC) systems. In such configurations, fiber optic cables carry signals over long distances, while the coaxial cable handles the last mile of signal delivery.

Additionally, coaxial cables are utilized in audio-video systems and surveillance (CCTV), where their resistance to interference and low signal attenuation allow the transmission of high-quality images and sound. In the context of security monitoring, their stability and reliability are critical, making them the preferred solution in many surveillance systems. Discovering and understanding these applications of coaxial cables enables effective use in various projects, both for hobbyists and professionals in electronics and telecommunications.

What Are the Types of Coaxial Cables

Coaxial cables can be classified in various ways, including by characteristic impedance, which is crucial for their use in telecommunications. The most popular values are 50Ω and 75Ω. 50Ω cables are often used in radio environments and in applications involving high frequencies, such as wireless communication systems. Meanwhile, 75Ω cables are primarily used in cable television and video signal transmission systems, where their design ensures better image and sound quality.

Different types of coaxial cables also play an important role in adapting to specific needs. Hard-line cables feature a rigid design, making them ideal for transmission and antenna connections, especially in large-scale installations. Flexible cables are more pliable and easier to install, making them suitable for use in challenging conditions. Semi-rigid cables combine characteristics of both types, offering a compromise between rigidity and flexibility. This knowledge enables achieving optimal performance in telecommunications systems.

What Are the Key Technical Parameters

When it comes to coaxial cables, understanding key technical parameters that define their performance and application is important. Characteristic impedance is one of the most important attributes, with standard values of 50Ω and 75Ω. Choosing the correct impedance is crucial to avoid signal reflections and ensure transmission efficiency. 50Ω cables are most commonly used in radio technology, while 75Ω cables are standard in cable television.

Another important parameter is signal attenuation, which describes how much signal is lost during transmission. Generally, larger cable diameters lead to lower attenuation, which is critical when working with high frequencies. The type of dielectric also affects attenuation; for example, cables with Teflon dielectric offer better properties compared to standard polyethylene.

Shielding effectiveness is another key parameter that indicates how well the cable protects the signal from electromagnetic interference. High-quality coaxial cables employ various shielding techniques, enabling more stable signal transmission, especially in challenging environments.

Finally, bandwidth is the frequency range over which the cable can effectively transmit signals. Coaxial cables can carry signals from low to very high frequencies, making them versatile in different telecommunications applications.

How to Install Coaxial Cables

Installing coaxial cables requires consideration of several key guidelines to ensure proper operation and longevity. First and foremost is the allowable bending radius. Coaxial cables should not be bent at too sharp an angle, as this can damage their structure and increase signal attenuation. Typically, the allowable bending radius ranges from 10 to 20 times the cable diameter. Therefore, it is advisable to plan the installation route with sufficient clearance to avoid unfavorable bends.

Another important rule is cable routing. Cables should be laid in a way that minimizes exposure to electromagnetic interference. Avoid placing coaxial cables near power or signal cables that may introduce noise. During operation, it is also important not to overload cables with excessive pressure or expose them to extreme weather conditions.

By following these rules, optimal performance of coaxial cables can be ensured, which is critical for maintaining signal quality. A well-planned installation will bring tangible benefits both in domestic and professional applications, guaranteeing telecommunications system reliability.

What Are the Advantages of Coaxial Cables

Coaxial cables offer a range of advantages that make them chosen for various telecommunications applications. First and foremost, they provide protection of the signal from electromagnetic interference, which is vital for signal stability. Thanks to shielding, these cables effectively minimize the impact of external sources of interference, which is especially important in densely populated or industrial areas.

Additionally, coaxial cables are characterized by resistance to mechanical damage. Their construction with a hard jacket enables them to withstand various impacts and pressures, making them an ideal solution for installations exposed to external forces. This increases their durability and reliability, which is crucial in industrial and infrastructural applications.

Last but not least, an important advantage is the ability to use coaxial cables in various environments. These cables perform excellently in both indoor and outdoor installations, and their design allows operation across a range of temperatures and humid conditions. Because of these features, coaxial cables remain a popular choice, especially in hybrid fiber-coaxial (HFC) networks, where they combine the benefits of both technologies.

What Are the Disadvantages of Coaxial Cables

Although coaxial cables have many advantages, they are also associated with certain drawbacks that should be considered before use. Primarily, installation challenges can be burdensome. These cables have limited flexibility, which makes installation in difficult conditions complicated. The thicker the conductor, the harder it is to route, potentially causing delays and increased labor costs.

Another issue is signal loss over long distances. While coaxial cables can operate over extended lengths, their efficiency gradually declines. Therefore, in large installations, using additional signal amplifiers may be necessary, increasing system complexity and costs.

Finally, coaxial cables are sensitive to environmental factors. Exposure to high temperatures, moisture, or chemicals can negatively affect their performance. For this reason, using them in extreme conditions or highly contaminated locations can be problematic. These disadvantages should be kept in mind when planning coaxial cable applications in various telecommunications systems.

What to Know About the Future of Coaxial Cables

The future of coaxial cables looks promising despite the development of modern technologies such as fiber optics and wireless communications. Current applications and innovations include their integration in hybrid fiber-coaxial (HFC) networks, where fiber optic cables handle long-distance transport, and coaxial cables deliver signals directly to homes and businesses. Additionally, modern standards like DOCSIS 3.1/4.0 enable data transmission at several gigabits per second over conventional coaxial cables. This keeps these cables competitive against FTTH (fiber-to-the-home) solutions.

Another significant trend is integration with new technologies, including 5G. Coaxial cables are used in power supply and signal transmission systems, bringing convenience and reducing the number of required cables. In the 5G context, the use of coaxial cables in small base stations is gaining importance, as they can transmit high-frequency signals and power devices. Automation and vision systems in industry also benefit from the reliability provided by coaxial cables, which makes their role in modern communication infrastructure continue to grow.

Summary

Coaxial cables, though not the newest technology, play a key role in modern communication infrastructure. Thanks to their ability to transmit high-frequency signals with minimal interference, they are invaluable in telecommunications, television, and automation systems. This article detailed their construction, operation, and applications, enabling an understanding of how to effectively use these cables in practice.

We encourage further exploration of the topic to better tailor solutions to individual needs. Whether you are a hobbyist, student, or professional, choosing the right coaxial cable can significantly affect project quality.

FAQ – frequently asked questions about coaxial cables

What are the main applications of coaxial cables?

Coaxial cables are widely used in telecommunications for the transmission of radio and digital signals. They are also used in antenna installations, cable television, as well as audio-video and monitoring (CCTV) systems due to their resistance to electromagnetic interference.

How do coaxial cables with different impedances differ?

Coaxial cables have different characteristic impedances – the most common are 50Ω and 75Ω. 50Ω cables are ideal for radio environments and high-frequency applications, while 75Ω cables are mainly used in cable television, where they provide better image and sound quality.

What are the key technical parameters of coaxial cables?

The key technical parameters of coaxial cables include characteristic impedance, signal attenuation (signal loss during transmission), shielding effectiveness (protection against electromagnetic interference), and bandwidth (the range of frequencies over which the cable can effectively transmit signals).

How to properly install coaxial cables?

Installing coaxial cables requires following several rules, such as avoiding excessive bending (the permissible bending radius should be 10–20 times the cable diameter) and minimizing exposure to electromagnetic interference through proper cable routing. It is also important to avoid mechanical stress on the cables.

What are the disadvantages of coaxial cables?

Among the disadvantages of coaxial cables are installation challenges related to their stiffness, signal losses over long distances, and sensitivity to environmental factors such as high temperatures and humidity, which may affect their performance.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO