+1 500 000 のオファーにある商品数

7000 個の小包が毎日発送されます

150 カ国からの +300 000 の顧客

Quick Buy お気に入り
カート

MACTRONIC

MACTRONIC is a Polish company established in the 1980s, which specializes in the production of flashlights. It is the Polish leader in its field and one of the largest manufacturers of lighting equipment in Europe. Flashlights by MACTRONIC are high quality devices, designed for use by both professionals and hobbyists. They can be found in households, on hiking trails or attached to bicycles.

MACTRONIC offers 500 different models of flashlights, many of which are based on company’s own industrial designs. Numerous research and tests confirm the high quality of solutions offered by MACTRONIC.