+1 500 000 のオファーにある商品数

7000 個の小包が毎日発送されます

150 カ国からの +320 000 の顧客

Quick Buy お気に入り
カート

ONSEMI

ON Semiconductor was established in 1999. It is a spinoff unit from Motorola and is now one of the leading manufacturers of semiconductors. ON Semiconductor offers a wide range of solutions for signal processing, discrete and logical components, communication solutions, LED lighting solutions, consumer electronics, computers, home appliances, as well as products for medical and military applications. Image sensors and radar solutions for the automotive market are also an important part of the On Semiconductor offer.

The company is seated in Phoenix (USA), but thanks to its development strategy based on acquisitions, it now has an extensive network of plants, development centres and offices in North America, Europe and the East Asia. The acquired companies include both manufacturing and technology companies, such as LSI Logistic, Catalyst Semiconductor, Sanyo Semiconductor, CMOS Sensor Business Unit from Cypress Semiconductor, Aptina and Fairchild Semiconductor.

The main product groups offered by ON Semiconductor are semiconductor diodes, Bridge rectifiers, bipolar transistors, FET and IGBT transistors, thyristors, voltage regulators and stabilizers, AC/DC converters, DC/DC converters, voltage converters, drivers and controllers, supervisor circuits and timers, current and voltage management systems, logic circuits and clock modules, data communication systems, memories, microcontrollers, signal converters, amplifiers and analogue comparators, analogue switches, interfaces, image converters and radar systems.