+1 500 000 のオファーにある商品数

7000 個の小包が毎日発送されます

150 カ国からの +300 000 の顧客

Quick Buy お気に入り
カート

WIKA

WIKA is a recognized global market leader in measurement technology. The company was created in 1946 in Germany. WIKA is a global market leader in pressure, temperature, level and force measurement, as well as in calibration. This brands’ manometers, sensors and thermostats are used in i.e. food, petrochemical, heating, refrigeration and heating industries. WIKA has 43 subsidiaries that include manufacturing plants, service&maintenance facilities and teams responsible for additional services.

In the TME offer we can find e.g. sensors and transducers, thermostats and also measurement components by WIKA.