+1 500 000 のオファーにある商品数
7000 個の小包が毎日発送されます
150 カ国からの +300 000 の顧客
発行日: 16-05-2019 更新日: 10-04-2026 🕒 3 分钟阅读
Appropriately selected inductive sensor serves as the basis for properly operating technological line and for devices using this kind of automation components everyday. Currently, sensors are responsible for measurements, localising metal objects, counting, or drawing up transport routes in numerous manufacturing industries. Automatic control of machines and devices within production lines is based on proximity sensors.
From technical perspective, this is quite complicated, but you don’t have to know the characteristics of a sensor in order to understand how it works. The sensor works by detecting any changes in the position of metal objects in its surroundings, and by sending signal (information) about the location of the object. One of the advantages of inductive sensors is touchless operation, which distinguishes them from contact sensors that require direct contact with the object.
Currently, manufacturing companies provide a wide range of automation components based on basic parameters.
Inductive sensor package indicates the shape of the component, which in the case of cylindrical sensors (oval shape) has metric thread pitch enabling easy mounting. Thanks to this, the user can choose thread size or diameter based on the measurement table (e.g. cylindrical sensor M12 or ϕ12). Inductive sensors with packages in the shape of a cuboid are also available.
International Protection Rating describes package’s resistance to external factors in accordance with the IEC 60 529 (PN-EN 60 529) standard. In the string (IP XX), the first number represents the degree of protection against solids and contact, and the second number represents the degree of water infiltration into the device. Depending on the environment and operating conditions, an appropriate degree of protection is selected. In more demanding operating conditions, the device is exposed to external factors, therefore the degree of protection should be selected in such a way to ensure optimal working conditions for the sensor. The basic and most commonly found degree of protection is IP67, which ensures complete protection against dust (dust tight) and protection of the device when it is immersed in water up to 1 m for a defined short time (a few minutes). Similarly to the degree of tightness, the lifetime of a sensor can also be extended by selecting an appropriate material. Knowing the operating mode and working conditions of an inductive sensor lets you choose the material with appropriate properties. Currently, the most popular are stainless steel or brass sensors.
Supply voltage determines the amount of voltage required for the correct operation of the device. Inductive sensors can be powered with DC or AC current. Based on the design of the particular technological line, the user selects the voltage.
Unlike contact sensors, inductive sensors use the range to determine the position of a monitored object. In reality, this extends the lifetime of a component by eliminating factors occurring in the contact between the sensor and the object. In technological lines, the distance between the sensor and the object are often in millimetres.
Output configuration determines the types of outputs of an inductive sensor, and consequently the type of the output signal. Inductive sensors are available in two-, three-, or four-wire versions. The most commonly used are three-wire sensors. They feature two wires responsible for providing power, and a binary signal, connected to a driver. In order to understand the output configuration of an inductive sensor, one needs to pay attention to the type of bipolar transistor used by the device (PNP transistor – positive output, NPN transistor - negative output). Depending on the configuration of the transistor, it can be enabled after detecting an object (normally open, NO), or when no object is detected (normally closed, NC). Types of output signal configuration:
PNP NO (the sensor puts high signal on the output when it detects an object)
PNP NC (the sensor puts high signal on the output when it does not detect an object)
NPN NO (the sensor puts low signal on the output when it detects an object)
NPN NC (the sensor puts low signal on the output when it does not detect an object)
Depending on the output signal that you need, you can also choose a sensor that provides analogue signal from the 4-20mA, 1-9V range.
Transfer Multisort Elektronik(TME)は、電子部品、電気・電子機器、作業工具、ならびに産業用オートメーション機器を取り扱う世界有数のグローバルディストリビューターです。TMEのカタログには、1300社以上の主要メーカーによる150万点を超える製品が掲載されています。ウッチ市およびルズグフ市に所在するTMEの最新物流センターは、総面積40,000㎡以上を有し、毎日約6,000個の電子部品関連パッケージを、150か国以上の顧客へ発送しています。
TME はまた、TME Education プロジェクトを通じて若手エンジニアや電子工学愛好家の知識とスキルの向上に取り組み、TechMasterEvent シリーズを開催して技術コミュニティを支援し、イノベーションと経験の共有を促進しています。