+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

축전기

(14 873)

A capacitor is one of the basic passive electronic components. Its task is to store energy in the electric field. The amount of stored energy is described by the capacitance of the capacitor, which is expressed in farads (F). The capacitance measured in full farads is not very common. Typically, capacitors have the capacitance of micro- (µ), nano- (n), pico- (p) farads.
The second basic parameter of a capacitor, apart from its capacitance, is its maximum operating voltage. Due to its design, a capacitor is susceptible to the so-called breakdown. Therefore, each capacitor has a parameter that defines the maximum voltage that can appear between its terminals. After exceeding it, a breakdown may occur, resulting in a short-circuit of the capacitor.

Capacitor – design and principle of operation

Capacitors are made of two conductors (capacitor plates) separated from each other by a non-conductive dielectric material. It can be any insulating material such as: air, plastic, ceramics, paper. The operation of a capacitor is based on Coulomb's law. According to that law, the media on both plates of the capacitor interact with each other. Media with the same charge repel each other, while those with the opposite charge attract each other. The effect of such a phenomenon is the presence of opposite charges on the capacitor plates. Their number is equal on both sides. Thanks to the dielectric material contained between the plates, the flow of charges is impossible, and this results in the formation of an electric field.

Types of capacitors

There are many different types of capacitors available on the market, including customized designs for specific tasks. Some of the types of capacitors available at TME are described below. Ceramic capacitors and MLCCs – these are some of the most common electronic components. What is interesting, the number of such capacitors manufactured in a single year is about one trillion. Ceramic capacitors owe their name to the ceramics used as an insulating material. MLCCs (multi-layer ceramic capacitors) are a subtype of conventional ceramic capacitors. An MLCC is a ceramic capacitor made in a multi-layer process. Ceramic capacitors do not have a specific polarisation, so they can be used in AC circuits, they are also available in both THT (through-hole mounting) and SMD (surface mounting) versions.

Electrolytic capacitors – the second most common type of capacitors are electrolytic designs. Thanks to the use of electrolyte, they offer much larger capacitance than ceramic capacitors. Almost all of them require appropriate polarisation – incorrect incorporation of such a capacitor into a circuit may even result in its explosion. These capacitors are also available in THT and SMD versions.

Trimmer – it is a variable capacitor, also called a tuning capacitor or tuning condenser. As the name suggests, the capacitance of such a capacitor can be freely adjusted. Trimmers were used in older designs of radios. At TME, several modern SMD trimmers are available.

Supercapacitors – they are a type of electrolytic capacitors and are able to store huge amounts of energy. Thanks to a special design, their capacitance reaches up to 3kF. In practice, it can be said that supercapacitors combine features of conventional capacitors and rechargeable batteries. Charging speed is their great advantage.

제품: 14 873

창고:

TME
전부
페이지 1
EEHZA1K470V | 커패시터: 하이브리드; H: 10.5mm; 47uF; 80VDC; 1.7A; SMD; ESR: 36mΩ; ZA; ±20%
커패시터: 하이브리드; H: 10.5mm; 47uF; 80VDC; 1.7A; SMD; ESR: 36mΩ; ZA; ±20%
제조업체 부품 번호: EEHZA1K470V
제조사: PANASONIC
다음의 수량에 대한 순 가격 1 pcs - 2.42 USD다음의 수량에 대한 총 가격 1 pcs - 2.42 USD
다음의 수량에 대한 순 가격 5 pcs - 1.46 USD다음의 수량에 대한 총 가격 5 pcs - 1.46 USD
다음의 수량에 대한 순 가격 10 pcs - 1.33 USD다음의 수량에 대한 총 가격 10 pcs - 1.33 USD
다음의 수량에 대한 순 가격 50 pcs - 1.11 USD다음의 수량에 대한 총 가격 50 pcs - 1.11 USD
다음의 수량에 대한 순 가격 100 pcs - 1.03 USD다음의 수량에 대한 총 가격 100 pcs - 1.03 USD
다음의 수량에 대한 순 가격 250 pcs - 0.93 USD다음의 수량에 대한 총 가격 250 pcs - 0.93 USD
다음의 수량에 대한 순 가격 500 pcs - 0.86 USD다음의 수량에 대한 총 가격 500 pcs - 0.86 USD
다음의 수량에 대한 순 가격 1000 pcs - 0.80 USD다음의 수량에 대한 총 가격 1000 pcs - 0.80 USD
다음의 수량에 대한 순 가격 1500 pcs - 0.77 USD다음의 수량에 대한 총 가격 1500 pcs - 0.77 USD
다음의 수량에 대한 순 가격 3500 pcs - 0.70 USD다음의 수량에 대한 총 가격 3500 pcs - 0.70 USD
28 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
MSASU31LBB5106KTNA01 | 커패시터: 세라믹; MLCC; 10uF; 50VDC; X5R; ±10%; SMD; 1206
커패시터: 세라믹; MLCC; 10uF; 50VDC; X5R; ±10%; SMD; 1206
제조업체 부품 번호: MSASU31LBB5106KTNA01
제조사: TAIYO YUDEN
다음의 수량에 대한 순 가격 1 pcs - 0.28 USD다음의 수량에 대한 총 가격 1 pcs - 0.28 USD
다음의 수량에 대한 순 가격 10 pcs - 0.15 USD다음의 수량에 대한 총 가격 10 pcs - 0.15 USD
다음의 수량에 대한 순 가격 50 pcs - 0.08 USD다음의 수량에 대한 총 가격 50 pcs - 0.08 USD
다음의 수량에 대한 순 가격 100 pcs - 0.06 USD다음의 수량에 대한 총 가격 100 pcs - 0.06 USD
다음의 수량에 대한 순 가격 250 pcs - 0.06 USD다음의 수량에 대한 총 가격 250 pcs - 0.06 USD
다음의 수량에 대한 순 가격 500 pcs - 0.05 USD다음의 수량에 대한 총 가격 500 pcs - 0.05 USD
다음의 수량에 대한 순 가격 1000 pcs - 0.05 USD다음의 수량에 대한 총 가격 1000 pcs - 0.05 USD
다음의 수량에 대한 순 가격 2000 pcs - 0.05 USD다음의 수량에 대한 총 가격 2000 pcs - 0.05 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
거의 사용할 수 없는 제품
NXH35VB220M3.5TP8X11.5 | 커패시터: 전해질; low ESR; THT; 220uF; 35VDC; Ø8x11.5mm; 피치: 3.5mm; ±20%
커패시터: 전해질; low ESR; THT; 220uF; 35VDC; Ø8x11.5mm; 피치: 3.5mm; ±20%
제조업체 부품 번호: NXH35VB220M3.5TP8X11.5
제조사: SAMYOUNG
다음의 수량에 대한 순 가격 1 pcs - 0.09 USD다음의 수량에 대한 총 가격 1 pcs - 0.09 USD
다음의 수량에 대한 순 가격 10 pcs - 0.08 USD다음의 수량에 대한 총 가격 10 pcs - 0.08 USD
다음의 수량에 대한 순 가격 50 pcs - 0.07 USD다음의 수량에 대한 총 가격 50 pcs - 0.07 USD
다음의 수량에 대한 순 가격 100 pcs - 0.07 USD다음의 수량에 대한 총 가격 100 pcs - 0.07 USD
다음의 수량에 대한 순 가격 250 pcs - 0.06 USD다음의 수량에 대한 총 가격 250 pcs - 0.06 USD
다음의 수량에 대한 순 가격 500 pcs - 0.06 USD다음의 수량에 대한 총 가격 500 pcs - 0.06 USD
다음의 수량에 대한 순 가격 1000 pcs - 0.06 USD다음의 수량에 대한 총 가격 1000 pcs - 0.06 USD
201 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
HG2W687M35050HC | 커패시터: 전해질; SNAP-IN; 680uF; 450VDC; Ø35x50mm; 피치: 10mm; ±20%; 터미널 수: 2
커패시터: 전해질; SNAP-IN; 680uF; 450VDC; Ø35x50mm; 피치: 10mm; ±20%; 터미널 수: 2
제조업체 부품 번호: HG2W687M35050HC
제조사: SAMWHA
다음의 수량에 대한 순 가격 1 pcs - 6.31 USD다음의 수량에 대한 총 가격 1 pcs - 6.31 USD
다음의 수량에 대한 순 가격 5 pcs - 6.03 USD다음의 수량에 대한 총 가격 5 pcs - 6.03 USD
다음의 수량에 대한 순 가격 10 pcs - 5.74 USD다음의 수량에 대한 총 가격 10 pcs - 5.74 USD
다음의 수량에 대한 순 가격 25 pcs - 5.44 USD다음의 수량에 대한 총 가격 25 pcs - 5.44 USD
다음의 수량에 대한 순 가격 50 pcs - 5.25 USD다음의 수량에 대한 총 가격 50 pcs - 5.25 USD
다음의 수량에 대한 순 가격 100 pcs - 4.98 USD다음의 수량에 대한 총 가격 100 pcs - 4.98 USD
175 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
GRM188R60J476ME01V | 커패시터: 세라믹; MLCC; 47uF; 6.3V; X5R; ±20%; SMD; 0603; 330mm
커패시터: 세라믹; MLCC; 47uF; 6.3V; X5R; ±20%; SMD; 0603; 330mm
제조업체 부품 번호: GRM188R60J476ME01V
제조사: MURATA
다음의 수량에 대한 순 가격 30000 pcs - 0.08 USD다음의 수량에 대한 총 가격 30000 pcs - 0.08 USD
0 TME에 재고 있음
개 번호 (다양성: 30 000)
최소 주문 수량: 30 000.
다수: 30 000.
NXA25VB100M2.5TP6.3X11 | 커패시터: 전해질; low ESR; THT; 100uF; 25VDC; Ø6.3x11mm; 피치: 2.5mm; ±20%
커패시터: 전해질; low ESR; THT; 100uF; 25VDC; Ø6.3x11mm; 피치: 2.5mm; ±20%
제조업체 부품 번호: NXA25VB100M2.5TP6.3X11
제조사: SAMYOUNG
다음의 수량에 대한 순 가격 1 pcs - 0.09 USD다음의 수량에 대한 총 가격 1 pcs - 0.09 USD
다음의 수량에 대한 순 가격 10 pcs - 0.05 USD다음의 수량에 대한 총 가격 10 pcs - 0.05 USD
다음의 수량에 대한 순 가격 50 pcs - 0.05 USD다음의 수량에 대한 총 가격 50 pcs - 0.05 USD
다음의 수량에 대한 순 가격 100 pcs - 0.04 USD다음의 수량에 대한 총 가격 100 pcs - 0.04 USD
다음의 수량에 대한 순 가격 250 pcs - 0.04 USD다음의 수량에 대한 총 가격 250 pcs - 0.04 USD
다음의 수량에 대한 순 가격 500 pcs - 0.04 USD다음의 수량에 대한 총 가격 500 pcs - 0.04 USD
다음의 수량에 대한 순 가격 1000 pcs - 0.04 USD다음의 수량에 대한 총 가격 1000 pcs - 0.04 USD
다음의 수량에 대한 순 가격 1500 pcs - 0.03 USD다음의 수량에 대한 총 가격 1500 pcs - 0.03 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
SD2A106M05011PC | 커패시터: 전해질; THT; 10uF; 100VDC; Ø5x11mm; ±20%; 2000h; -40÷105°C; SD
커패시터: 전해질; THT; 10uF; 100VDC; Ø5x11mm; ±20%; 2000h; -40÷105°C; SD
제조업체 부품 번호: SD2A106M05011PC
제조사: SAMWHA
다음의 수량에 대한 순 가격 1 pcs - 0.09 USD다음의 수량에 대한 총 가격 1 pcs - 0.09 USD
다음의 수량에 대한 순 가격 10 pcs - 0.05 USD다음의 수량에 대한 총 가격 10 pcs - 0.05 USD
다음의 수량에 대한 순 가격 100 pcs - 0.02 USD다음의 수량에 대한 총 가격 100 pcs - 0.02 USD
다음의 수량에 대한 순 가격 500 pcs - 0.02 USD다음의 수량에 대한 총 가격 500 pcs - 0.02 USD
다음의 수량에 대한 순 가격 1000 pcs - 0.02 USD다음의 수량에 대한 총 가격 1000 pcs - 0.02 USD
다음의 수량에 대한 순 가격 2000 pcs - 0.02 USD다음의 수량에 대한 총 가격 2000 pcs - 0.02 USD
다음의 수량에 대한 순 가격 4000 pcs - 0.02 USD다음의 수량에 대한 총 가격 4000 pcs - 0.02 USD
다음의 수량에 대한 순 가격 6000 pcs - 0.02 USD다음의 수량에 대한 총 가격 6000 pcs - 0.02 USD
다음의 수량에 대한 순 가격 10000 pcs - 0.01 USD다음의 수량에 대한 총 가격 10000 pcs - 0.01 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
RD1C108M10016PA | 커패시터: 전해질; THT; 1000uF; 16VDC; Ø10x16mm; ±20%; 2000h; -55÷105°C; RD
커패시터: 전해질; THT; 1000uF; 16VDC; Ø10x16mm; ±20%; 2000h; -55÷105°C; RD
제조업체 부품 번호: RD1C108M10016PA
제조사: SAMWHA
다음의 수량에 대한 순 가격 1 pcs - 0.09 USD다음의 수량에 대한 총 가격 1 pcs - 0.09 USD
다음의 수량에 대한 순 가격 10 pcs - 0.08 USD다음의 수량에 대한 총 가격 10 pcs - 0.08 USD
다음의 수량에 대한 순 가격 50 pcs - 0.08 USD다음의 수량에 대한 총 가격 50 pcs - 0.08 USD
다음의 수량에 대한 순 가격 100 pcs - 0.07 USD다음의 수량에 대한 총 가격 100 pcs - 0.07 USD
다음의 수량에 대한 순 가격 250 pcs - 0.07 USD다음의 수량에 대한 총 가격 250 pcs - 0.07 USD
다음의 수량에 대한 순 가격 500 pcs - 0.07 USD다음의 수량에 대한 총 가격 500 pcs - 0.07 USD
다음의 수량에 대한 순 가격 1000 pcs - 0.06 USD다음의 수량에 대한 총 가격 1000 pcs - 0.06 USD
다음의 수량에 대한 순 가격 1500 pcs - 0.06 USD다음의 수량에 대한 총 가격 1500 pcs - 0.06 USD
다음의 수량에 대한 순 가격 3000 pcs - 0.06 USD다음의 수량에 대한 총 가격 3000 pcs - 0.06 USD
다음의 수량에 대한 순 가격 6000 pcs - 0.05 USD다음의 수량에 대한 총 가격 6000 pcs - 0.05 USD
816 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
SS1J106M05007PC | 커패시터: 전해질; THT; 10uF; 63VDC; Ø5x7mm; ±20%; 2000h; -40÷105°C; SS; H: 7mm
커패시터: 전해질; THT; 10uF; 63VDC; Ø5x7mm; ±20%; 2000h; -40÷105°C; SS; H: 7mm
제조업체 부품 번호: SS1J106M05007PC
제조사: SAMWHA
다음의 수량에 대한 순 가격 10 pcs - 0.07 USD다음의 수량에 대한 총 가격 10 pcs - 0.07 USD
다음의 수량에 대한 순 가격 50 pcs - 0.04 USD다음의 수량에 대한 총 가격 50 pcs - 0.04 USD
다음의 수량에 대한 순 가격 100 pcs - 0.03 USD다음의 수량에 대한 총 가격 100 pcs - 0.03 USD
다음의 수량에 대한 순 가격 200 pcs - 0.03 USD다음의 수량에 대한 총 가격 200 pcs - 0.03 USD
다음의 수량에 대한 순 가격 400 pcs - 0.03 USD다음의 수량에 대한 총 가격 400 pcs - 0.03 USD
다음의 수량에 대한 순 가격 1000 pcs - 0.03 USD다음의 수량에 대한 총 가격 1000 pcs - 0.03 USD
다음의 수량에 대한 순 가격 2000 pcs - 0.03 USD다음의 수량에 대한 총 가격 2000 pcs - 0.03 USD
0 TME에 재고 있음
개 번호 (다양성: 10)
최소 주문 수량: 10.
다수: 10.
NXH50VB470M10X20 | 커패시터: 전해질; low ESR; THT; 470uF; 50VDC; Ø10x20mm; 피치: 5mm; ±20%; 10000h
커패시터: 전해질; low ESR; THT; 470uF; 50VDC; Ø10x20mm; 피치: 5mm; ±20%; 10000h
제조업체 부품 번호: NXH50VB470M10X20
제조사: SAMYOUNG
다음의 수량에 대한 순 가격 1 pcs - 0.25 USD다음의 수량에 대한 총 가격 1 pcs - 0.25 USD
다음의 수량에 대한 순 가격 10 pcs - 0.21 USD다음의 수량에 대한 총 가격 10 pcs - 0.21 USD
다음의 수량에 대한 순 가격 25 pcs - 0.19 USD다음의 수량에 대한 총 가격 25 pcs - 0.19 USD
다음의 수량에 대한 순 가격 50 pcs - 0.17 USD다음의 수량에 대한 총 가격 50 pcs - 0.17 USD
다음의 수량에 대한 순 가격 100 pcs - 0.16 USD다음의 수량에 대한 총 가격 100 pcs - 0.16 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
NXH16VB470M8X11.5 | 커패시터: 전해질; low ESR; THT; 470uF; 16VDC; Ø8x11.5mm; 피치: 3.5mm; ±20%
커패시터: 전해질; low ESR; THT; 470uF; 16VDC; Ø8x11.5mm; 피치: 3.5mm; ±20%
제조업체 부품 번호: NXH16VB470M8X11.5
제조사: SAMYOUNG
다음의 수량에 대한 순 가격 1 pcs - 0.11 USD다음의 수량에 대한 총 가격 1 pcs - 0.11 USD
다음의 수량에 대한 순 가격 10 pcs - 0.08 USD다음의 수량에 대한 총 가격 10 pcs - 0.08 USD
다음의 수량에 대한 순 가격 25 pcs - 0.07 USD다음의 수량에 대한 총 가격 25 pcs - 0.07 USD
다음의 수량에 대한 순 가격 50 pcs - 0.07 USD다음의 수량에 대한 총 가격 50 pcs - 0.07 USD
다음의 수량에 대한 순 가격 100 pcs - 0.06 USD다음의 수량에 대한 총 가격 100 pcs - 0.06 USD
다음의 수량에 대한 순 가격 200 pcs - 0.06 USD다음의 수량에 대한 총 가격 200 pcs - 0.06 USD
572 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
GRM188R61E106KA73V | 커패시터: 세라믹; MLCC; 10uF; 25V; X5R; ±10%; SMD; 0603; 330mm
커패시터: 세라믹; MLCC; 10uF; 25V; X5R; ±10%; SMD; 0603; 330mm
제조업체 부품 번호: GRM188R61E106KA73V
제조사: MURATA
다음의 수량에 대한 순 가격 30000 pcs - 0.03 USD다음의 수량에 대한 총 가격 30000 pcs - 0.03 USD
0 TME에 재고 있음
개 번호 (다양성: 30 000)
최소 주문 수량: 30 000.
다수: 30 000.
거의 사용할 수 없는 제품
NXH35VB47M5X11 | 커패시터: 전해질; low ESR; THT; 47uF; 35VDC; Ø5x11mm; 피치: 2mm; ±20%; 6000h
커패시터: 전해질; low ESR; THT; 47uF; 35VDC; Ø5x11mm; 피치: 2mm; ±20%; 6000h
제조업체 부품 번호: NXH35VB47M5X11
제조사: SAMYOUNG
다음의 수량에 대한 순 가격 1 pcs - 0.11 USD다음의 수량에 대한 총 가격 1 pcs - 0.11 USD
다음의 수량에 대한 순 가격 10 pcs - 0.06 USD다음의 수량에 대한 총 가격 10 pcs - 0.06 USD
다음의 수량에 대한 순 가격 25 pcs - 0.05 USD다음의 수량에 대한 총 가격 25 pcs - 0.05 USD
다음의 수량에 대한 순 가격 50 pcs - 0.05 USD다음의 수량에 대한 총 가격 50 pcs - 0.05 USD
다음의 수량에 대한 순 가격 100 pcs - 0.04 USD다음의 수량에 대한 총 가격 100 pcs - 0.04 USD
다음의 수량에 대한 순 가격 200 pcs - 0.04 USD다음의 수량에 대한 총 가격 200 pcs - 0.04 USD
125 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
WB1V108M12025PL | 커패시터: 전해질; THT; 1000uF; 35VDC; Ø12.5x25mm; ±20%; 5000h; -40÷105°C; WB
커패시터: 전해질; THT; 1000uF; 35VDC; Ø12.5x25mm; ±20%; 5000h; -40÷105°C; WB
제조업체 부품 번호: WB1V108M12025PL
제조사: SAMWHA
다음의 수량에 대한 순 가격 1 pcs - 0.38 USD다음의 수량에 대한 총 가격 1 pcs - 0.38 USD
다음의 수량에 대한 순 가격 10 pcs - 0.34 USD다음의 수량에 대한 총 가격 10 pcs - 0.34 USD
다음의 수량에 대한 순 가격 50 pcs - 0.32 USD다음의 수량에 대한 총 가격 50 pcs - 0.32 USD
다음의 수량에 대한 순 가격 100 pcs - 0.31 USD다음의 수량에 대한 총 가격 100 pcs - 0.31 USD
다음의 수량에 대한 순 가격 200 pcs - 0.29 USD다음의 수량에 대한 총 가격 200 pcs - 0.29 USD
다음의 수량에 대한 순 가격 400 pcs - 0.28 USD다음의 수량에 대한 총 가격 400 pcs - 0.28 USD
다음의 수량에 대한 순 가격 800 pcs - 0.26 USD다음의 수량에 대한 총 가격 800 pcs - 0.26 USD
다음의 수량에 대한 순 가격 1600 pcs - 0.25 USD다음의 수량에 대한 총 가격 1600 pcs - 0.25 USD
1138 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
NXH35VB470M10X16 | 커패시터: 전해질; low ESR; THT; 470uF; 35VDC; Ø10x16mm; 피치: 5mm; ±20%; 10000h
커패시터: 전해질; low ESR; THT; 470uF; 35VDC; Ø10x16mm; 피치: 5mm; ±20%; 10000h
제조업체 부품 번호: NXH35VB470M10X16
제조사: SAMYOUNG
다음의 수량에 대한 순 가격 1 pcs - 0.14 USD다음의 수량에 대한 총 가격 1 pcs - 0.14 USD
다음의 수량에 대한 순 가격 10 pcs - 0.13 USD다음의 수량에 대한 총 가격 10 pcs - 0.13 USD
다음의 수량에 대한 순 가격 25 pcs - 0.11 USD다음의 수량에 대한 총 가격 25 pcs - 0.11 USD
다음의 수량에 대한 순 가격 50 pcs - 0.09 USD다음의 수량에 대한 총 가격 50 pcs - 0.09 USD
다음의 수량에 대한 순 가격 100 pcs - 0.09 USD다음의 수량에 대한 총 가격 100 pcs - 0.09 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
MSASU168AB7105KTNA01 | 커패시터: 세라믹; MLCC; 1uF; 50VDC; X7R; ±10%; SMD; 0603
커패시터: 세라믹; MLCC; 1uF; 50VDC; X7R; ±10%; SMD; 0603
제조업체 부품 번호: MSASU168AB7105KTNA01
제조사: TAIYO YUDEN
다음의 수량에 대한 순 가격 1 pcs - 0.14 USD다음의 수량에 대한 총 가격 1 pcs - 0.14 USD
다음의 수량에 대한 순 가격 10 pcs - 0.05 USD다음의 수량에 대한 총 가격 10 pcs - 0.05 USD
다음의 수량에 대한 순 가격 100 pcs - 0.03 USD다음의 수량에 대한 총 가격 100 pcs - 0.03 USD
다음의 수량에 대한 순 가격 500 pcs - 0.02 USD다음의 수량에 대한 총 가격 500 pcs - 0.02 USD
다음의 수량에 대한 순 가격 1000 pcs - 0.02 USD다음의 수량에 대한 총 가격 1000 pcs - 0.02 USD
다음의 수량에 대한 순 가격 4000 pcs - 0.02 USD다음의 수량에 대한 총 가격 4000 pcs - 0.02 USD
99119 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
거의 사용할 수 없는 제품
NXH25VB1000M5.0TP10X25 | 커패시터: 전해질; low ESR; THT; 1000uF; 25VDC; Ø10x25mm; 피치: 5mm; ±20%; 18mΩ
커패시터: 전해질; low ESR; THT; 1000uF; 25VDC; Ø10x25mm; 피치: 5mm; ±20%; 18mΩ
제조업체 부품 번호: NXH25VB1000M5.0TP10X25
제조사: SAMYOUNG
다음의 수량에 대한 순 가격 1 pcs - 0.31 USD다음의 수량에 대한 총 가격 1 pcs - 0.31 USD
다음의 수량에 대한 순 가격 10 pcs - 0.26 USD다음의 수량에 대한 총 가격 10 pcs - 0.26 USD
다음의 수량에 대한 순 가격 50 pcs - 0.24 USD다음의 수량에 대한 총 가격 50 pcs - 0.24 USD
다음의 수량에 대한 순 가격 100 pcs - 0.22 USD다음의 수량에 대한 총 가격 100 pcs - 0.22 USD
다음의 수량에 대한 순 가격 250 pcs - 0.21 USD다음의 수량에 대한 총 가격 250 pcs - 0.21 USD
다음의 수량에 대한 순 가격 500 pcs - 0.19 USD다음의 수량에 대한 총 가격 500 pcs - 0.19 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
NXH35VB100M6.3X11 | 커패시터: 전해질; low ESR; THT; 100uF; 35VDC; Ø6.3x11mm; 피치: 2.5mm; ±20%
커패시터: 전해질; low ESR; THT; 100uF; 35VDC; Ø6.3x11mm; 피치: 2.5mm; ±20%
제조업체 부품 번호: NXH35VB100M6.3X11
제조사: SAMYOUNG
다음의 수량에 대한 순 가격 1 pcs - 0.13 USD다음의 수량에 대한 총 가격 1 pcs - 0.13 USD
다음의 수량에 대한 순 가격 10 pcs - 0.08 USD다음의 수량에 대한 총 가격 10 pcs - 0.08 USD
다음의 수량에 대한 순 가격 25 pcs - 0.06 USD다음의 수량에 대한 총 가격 25 pcs - 0.06 USD
다음의 수량에 대한 순 가격 50 pcs - 0.05 USD다음의 수량에 대한 총 가격 50 pcs - 0.05 USD
다음의 수량에 대한 순 가격 100 pcs - 0.05 USD다음의 수량에 대한 총 가격 100 pcs - 0.05 USD
다음의 수량에 대한 순 가격 200 pcs - 0.05 USD다음의 수량에 대한 총 가격 200 pcs - 0.05 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
NXH35VB1000M12.5X20 | 커패시터: 전해질; low ESR; THT; 1000uF; 35VDC; Ø12.5x20mm; 피치: 5mm; ±20%
커패시터: 전해질; low ESR; THT; 1000uF; 35VDC; Ø12.5x20mm; 피치: 5mm; ±20%
제조업체 부품 번호: NXH35VB1000M12.5X20
제조사: SAMYOUNG
다음의 수량에 대한 순 가격 1 pcs - 0.41 USD다음의 수량에 대한 총 가격 1 pcs - 0.41 USD
다음의 수량에 대한 순 가격 10 pcs - 0.35 USD다음의 수량에 대한 총 가격 10 pcs - 0.35 USD
다음의 수량에 대한 순 가격 25 pcs - 0.31 USD다음의 수량에 대한 총 가격 25 pcs - 0.31 USD
다음의 수량에 대한 순 가격 50 pcs - 0.28 USD다음의 수량에 대한 총 가격 50 pcs - 0.28 USD
다음의 수량에 대한 순 가격 100 pcs - 0.26 USD다음의 수량에 대한 총 가격 100 pcs - 0.26 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
MSAST21GBB5106MTNA01 | 커패시터: 세라믹; MLCC; 10uF; 25VDC; X5R; ±20%; SMD; 0805
커패시터: 세라믹; MLCC; 10uF; 25VDC; X5R; ±20%; SMD; 0805
제조업체 부품 번호: MSAST21GBB5106MTNA01
제조사: TAIYO YUDEN
다음의 수량에 대한 순 가격 1 pcs - 0.12 USD다음의 수량에 대한 총 가격 1 pcs - 0.12 USD
다음의 수량에 대한 순 가격 10 pcs - 0.07 USD다음의 수량에 대한 총 가격 10 pcs - 0.07 USD
다음의 수량에 대한 순 가격 100 pcs - 0.04 USD다음의 수량에 대한 총 가격 100 pcs - 0.04 USD
다음의 수량에 대한 순 가격 500 pcs - 0.04 USD다음의 수량에 대한 총 가격 500 pcs - 0.04 USD
다음의 수량에 대한 순 가격 1500 pcs - 0.03 USD다음의 수량에 대한 총 가격 1500 pcs - 0.03 USD
다음의 수량에 대한 순 가격 3000 pcs - 0.03 USD다음의 수량에 대한 총 가격 3000 pcs - 0.03 USD
307 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
거의 사용할 수 없는 제품
표준 오퍼에 포함되지 않은 제품에 대한 요청
요청이 성공적으로 전송되었습니다. 곧 제공된 이메일 주소로 제품 구매 제안서를 보내드리겠습니다.
고객 번호
제조업체 부품 번호
제조 업체
총액
이메일주소
메시지 내용