+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

축전기

(134 934)

A capacitor is one of the basic passive electronic components. Its task is to store energy in the electric field. The amount of stored energy is described by the capacitance of the capacitor, which is expressed in farads (F). The capacitance measured in full farads is not very common. Typically, capacitors have the capacitance of micro- (µ), nano- (n), pico- (p) farads.
The second basic parameter of a capacitor, apart from its capacitance, is its maximum operating voltage. Due to its design, a capacitor is susceptible to the so-called breakdown. Therefore, each capacitor has a parameter that defines the maximum voltage that can appear between its terminals. After exceeding it, a breakdown may occur, resulting in a short-circuit of the capacitor.

Capacitor – design and principle of operation

Capacitors are made of two conductors (capacitor plates) separated from each other by a non-conductive dielectric material. It can be any insulating material such as: air, plastic, ceramics, paper. The operation of a capacitor is based on Coulomb's law. According to that law, the media on both plates of the capacitor interact with each other. Media with the same charge repel each other, while those with the opposite charge attract each other. The effect of such a phenomenon is the presence of opposite charges on the capacitor plates. Their number is equal on both sides. Thanks to the dielectric material contained between the plates, the flow of charges is impossible, and this results in the formation of an electric field.

Types of capacitors

There are many different types of capacitors available on the market, including customized designs for specific tasks. Some of the types of capacitors available at TME are described below. Ceramic capacitors and MLCCs – these are some of the most common electronic components. What is interesting, the number of such capacitors manufactured in a single year is about one trillion. Ceramic capacitors owe their name to the ceramics used as an insulating material. MLCCs (multi-layer ceramic capacitors) are a subtype of conventional ceramic capacitors. An MLCC is a ceramic capacitor made in a multi-layer process. Ceramic capacitors do not have a specific polarisation, so they can be used in AC circuits, they are also available in both THT (through-hole mounting) and SMD (surface mounting) versions.

Electrolytic capacitors – the second most common type of capacitors are electrolytic designs. Thanks to the use of electrolyte, they offer much larger capacitance than ceramic capacitors. Almost all of them require appropriate polarisation – incorrect incorporation of such a capacitor into a circuit may even result in its explosion. These capacitors are also available in THT and SMD versions.

Trimmer – it is a variable capacitor, also called a tuning capacitor or tuning condenser. As the name suggests, the capacitance of such a capacitor can be freely adjusted. Trimmers were used in older designs of radios. At TME, several modern SMD trimmers are available.

Supercapacitors – they are a type of electrolytic capacitors and are able to store huge amounts of energy. Thanks to a special design, their capacitance reaches up to 3kF. In practice, it can be said that supercapacitors combine features of conventional capacitors and rechargeable batteries. Charging speed is their great advantage.

제품: 134 934

창고:

TME
외부의
전부
페이지 1
EEHZA1V470P | 커패시터: 하이브리드; 47uF; 35VDC; 1.3A; SMD; ESR: 60mΩ; ZA; ±20%; Ø6.3x5.8mm
커패시터: 하이브리드; 47uF; 35VDC; 1.3A; SMD; ESR: 60mΩ; ZA; ±20%; Ø6.3x5.8mm
제조업체 부품 번호: EEHZA1V470P
제조사: PANASONIC
다음의 수량에 대한 순 가격 1 pcs - 1.38 USD다음의 수량에 대한 총 가격 1 pcs - 1.38 USD
다음의 수량에 대한 순 가격 10 pcs - 0.62 USD다음의 수량에 대한 총 가격 10 pcs - 0.62 USD
다음의 수량에 대한 순 가격 50 pcs - 0.43 USD다음의 수량에 대한 총 가격 50 pcs - 0.43 USD
다음의 수량에 대한 순 가격 100 pcs - 0.38 USD다음의 수량에 대한 총 가격 100 pcs - 0.38 USD
다음의 수량에 대한 순 가격 250 pcs - 0.33 USD다음의 수량에 대한 총 가격 250 pcs - 0.33 USD
다음의 수량에 대한 순 가격 500 pcs - 0.31 USD다음의 수량에 대한 총 가격 500 pcs - 0.31 USD
다음의 수량에 대한 순 가격 1000 pcs - 0.30 USD다음의 수량에 대한 총 가격 1000 pcs - 0.30 USD
3268 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
UFW1H101MPD | 커패시터: 전해질; THT; 100uF; 50VDC; Ø8x11.5mm; 피치: 3.5mm; ±20%; 2000h; UFW
커패시터: 전해질; THT; 100uF; 50VDC; Ø8x11.5mm; 피치: 3.5mm; ±20%; 2000h; UFW
제조업체 부품 번호: UFW1H101MPD
제조사: NICHICON
다음의 수량에 대한 순 가격 1 pcs - 0.32 USD다음의 수량에 대한 총 가격 1 pcs - 0.32 USD
다음의 수량에 대한 순 가격 5 pcs - 0.28 USD다음의 수량에 대한 총 가격 5 pcs - 0.28 USD
다음의 수량에 대한 순 가격 10 pcs - 0.26 USD다음의 수량에 대한 총 가격 10 pcs - 0.26 USD
다음의 수량에 대한 순 가격 15 pcs - 0.25 USD다음의 수량에 대한 총 가격 15 pcs - 0.25 USD
다음의 수량에 대한 순 가격 50 pcs - 0.21 USD다음의 수량에 대한 총 가격 50 pcs - 0.21 USD
다음의 수량에 대한 순 가격 100 pcs - 0.18 USD다음의 수량에 대한 총 가격 100 pcs - 0.18 USD
다음의 수량에 대한 순 가격 200 pcs - 0.16 USD다음의 수량에 대한 총 가격 200 pcs - 0.16 USD
다음의 수량에 대한 순 가격 1000 pcs - 0.14 USD다음의 수량에 대한 총 가격 1000 pcs - 0.14 USD
다음의 수량에 대한 순 가격 3000 pcs - 0.13 USD다음의 수량에 대한 총 가격 3000 pcs - 0.13 USD
다음의 수량에 대한 순 가격 12000 pcs - 0.12 USD다음의 수량에 대한 총 가격 12000 pcs - 0.12 USD
2074 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
JFX-3.3U/250 | 커패시터: 폴리프로필렌; 3.3uF; 250VDC; ±5%; Ø17.5x31.5mm; 리드 치수: Ø0.8x35mm
커패시터: 폴리프로필렌; 3.3uF; 250VDC; ±5%; Ø17.5x31.5mm; 리드 치수: Ø0.8x35mm
제조업체 부품 번호: JFX-3.3U/250
제조사: Jb Capacitors
다음의 수량에 대한 순 가격 1 pcs - 2.00 USD다음의 수량에 대한 총 가격 1 pcs - 2.00 USD
다음의 수량에 대한 순 가격 5 pcs - 1.85 USD다음의 수량에 대한 총 가격 5 pcs - 1.85 USD
다음의 수량에 대한 순 가격 25 pcs - 1.61 USD다음의 수량에 대한 총 가격 25 pcs - 1.61 USD
다음의 수량에 대한 순 가격 100 pcs - 1.43 USD다음의 수량에 대한 총 가격 100 pcs - 1.43 USD
634 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
0805B104K500CT | 커패시터: 세라믹; 100nF; 50V; X7R; ±10%; 0805
커패시터: 세라믹; 100nF; 50V; X7R; ±10%; 0805
제조업체 부품 번호: 0805B104K500CT
제조사: WALSIN
다음의 수량에 대한 순 가격 1 pcs - 0.12 USD다음의 수량에 대한 총 가격 1 pcs - 0.12 USD
다음의 수량에 대한 순 가격 10 pcs - 0.06 USD다음의 수량에 대한 총 가격 10 pcs - 0.06 USD
다음의 수량에 대한 순 가격 100 pcs - 0.03 USD다음의 수량에 대한 총 가격 100 pcs - 0.03 USD
다음의 수량에 대한 순 가격 1000 pcs - 0.01 USD다음의 수량에 대한 총 가격 1000 pcs - 0.01 USD
다음의 수량에 대한 순 가격 4000 pcs - 0.01 USD다음의 수량에 대한 총 가격 4000 pcs - 0.01 USD
다음의 수량에 대한 순 가격 20000 pcs - 0.01 USD다음의 수량에 대한 총 가격 20000 pcs - 0.01 USD
다음의 수량에 대한 순 가격 40000 pcs - 0.01 USD다음의 수량에 대한 총 가격 40000 pcs - 0.01 USD
다음의 수량에 대한 순 가격 80000 pcs - 0.01 USD다음의 수량에 대한 총 가격 80000 pcs - 0.01 USD
15784493 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
거의 사용할 수 없는 제품
JFX-2.2U/250 | 커패시터: 폴리프로필렌; 2.2uF; 250VDC; ±5%; Ø14.5x31.5mm; 리드 치수: Ø0.8x30mm
커패시터: 폴리프로필렌; 2.2uF; 250VDC; ±5%; Ø14.5x31.5mm; 리드 치수: Ø0.8x30mm
제조업체 부품 번호: JFX-2.2U/250
제조사: Jb Capacitors
다음의 수량에 대한 순 가격 1 pcs - 1.82 USD다음의 수량에 대한 총 가격 1 pcs - 1.82 USD
다음의 수량에 대한 순 가격 5 pcs - 1.69 USD다음의 수량에 대한 총 가격 5 pcs - 1.69 USD
다음의 수량에 대한 순 가격 25 pcs - 1.56 USD다음의 수량에 대한 총 가격 25 pcs - 1.56 USD
다음의 수량에 대한 순 가격 100 pcs - 1.40 USD다음의 수량에 대한 총 가격 100 pcs - 1.40 USD
402 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
TAJA106K016RNJ | 커패시터: 탄탈륨; 10uF; 16VDC; SMD; A; 1206; ±10%; -55÷125°C; TAJ; 180mm
커패시터: 탄탈륨; 10uF; 16VDC; SMD; A; 1206; ±10%; -55÷125°C; TAJ; 180mm
제조업체 부품 번호: TAJA106K016RNJ
제조사: KYOCERA AVX
다음의 수량에 대한 순 가격 1 pcs - 0.54 USD다음의 수량에 대한 총 가격 1 pcs - 0.54 USD
다음의 수량에 대한 순 가격 10 pcs - 0.19 USD다음의 수량에 대한 총 가격 10 pcs - 0.19 USD
다음의 수량에 대한 순 가격 50 pcs - 0.16 USD다음의 수량에 대한 총 가격 50 pcs - 0.16 USD
다음의 수량에 대한 순 가격 100 pcs - 0.15 USD다음의 수량에 대한 총 가격 100 pcs - 0.15 USD
다음의 수량에 대한 순 가격 500 pcs - 0.12 USD다음의 수량에 대한 총 가격 500 pcs - 0.12 USD
다음의 수량에 대한 순 가격 1000 pcs - 0.11 USD다음의 수량에 대한 총 가격 1000 pcs - 0.11 USD
다음의 수량에 대한 순 가격 2000 pcs - 0.11 USD다음의 수량에 대한 총 가격 2000 pcs - 0.11 USD
다음의 수량에 대한 순 가격 4000 pcs - 0.10 USD다음의 수량에 대한 총 가격 4000 pcs - 0.10 USD
다음의 수량에 대한 순 가격 6000 pcs - 0.10 USD다음의 수량에 대한 총 가격 6000 pcs - 0.10 USD
다음의 수량에 대한 순 가격 10000 pcs - 0.10 USD다음의 수량에 대한 총 가격 10000 pcs - 0.10 USD
458 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
거의 사용할 수 없는 제품
0603B104K500CT | 커패시터: 세라믹; 100nF; 50V; X7R; ±10%; 0603
커패시터: 세라믹; 100nF; 50V; X7R; ±10%; 0603
제조업체 부품 번호: 0603B104K500CT
제조사: WALSIN
다음의 수량에 대한 순 가격 1 pcs - 0.07 USD다음의 수량에 대한 총 가격 1 pcs - 0.07 USD
다음의 수량에 대한 순 가격 10 pcs - 0.03 USD다음의 수량에 대한 총 가격 10 pcs - 0.03 USD
다음의 수량에 대한 순 가격 100 pcs - 0.02 USD다음의 수량에 대한 총 가격 100 pcs - 0.02 USD
다음의 수량에 대한 순 가격 1000 pcs - 0.01 USD다음의 수량에 대한 총 가격 1000 pcs - 0.01 USD
다음의 수량에 대한 순 가격 4000 pcs - 0.00 USD다음의 수량에 대한 총 가격 4000 pcs - 0.00 USD
다음의 수량에 대한 순 가격 12000 pcs - 0.00 USD다음의 수량에 대한 총 가격 12000 pcs - 0.00 USD
다음의 수량에 대한 순 가격 20000 pcs - 0.00 USD다음의 수량에 대한 총 가격 20000 pcs - 0.00 USD
다음의 수량에 대한 순 가격 40000 pcs - 0.00 USD다음의 수량에 대한 총 가격 40000 pcs - 0.00 USD
다음의 수량에 대한 순 가격 80000 pcs - 0.00 USD다음의 수량에 대한 총 가격 80000 pcs - 0.00 USD
다음의 수량에 대한 순 가격 160000 pcs - 0.00 USD다음의 수량에 대한 총 가격 160000 pcs - 0.00 USD
11919717 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
거의 사용할 수 없는 제품
JFX-4.7U/250 | 커패시터: 폴리프로필렌; 4.7uF; 250VDC; ±5%; Ø20.5x31.5mm; 리드 치수: Ø0.8x35mm
커패시터: 폴리프로필렌; 4.7uF; 250VDC; ±5%; Ø20.5x31.5mm; 리드 치수: Ø0.8x35mm
제조업체 부품 번호: JFX-4.7U/250
제조사: Jb Capacitors
다음의 수량에 대한 순 가격 1 pcs - 3.25 USD다음의 수량에 대한 총 가격 1 pcs - 3.25 USD
다음의 수량에 대한 순 가격 5 pcs - 2.95 USD다음의 수량에 대한 총 가격 5 pcs - 2.95 USD
다음의 수량에 대한 순 가격 25 pcs - 2.56 USD다음의 수량에 대한 총 가격 25 pcs - 2.56 USD
다음의 수량에 대한 순 가격 100 pcs - 2.38 USD다음의 수량에 대한 총 가격 100 pcs - 2.38 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
UFW1H221MPD | 커패시터: 전해질; THT; 220uF; 50VDC; Ø10x12.5mm; 피치: 5mm; ±20%; 2000h; UFW
커패시터: 전해질; THT; 220uF; 50VDC; Ø10x12.5mm; 피치: 5mm; ±20%; 2000h; UFW
제조업체 부품 번호: UFW1H221MPD
제조사: NICHICON
다음의 수량에 대한 순 가격 1 pcs - 0.43 USD다음의 수량에 대한 총 가격 1 pcs - 0.43 USD
다음의 수량에 대한 순 가격 10 pcs - 0.25 USD다음의 수량에 대한 총 가격 10 pcs - 0.25 USD
다음의 수량에 대한 순 가격 50 pcs - 0.21 USD다음의 수량에 대한 총 가격 50 pcs - 0.21 USD
다음의 수량에 대한 순 가격 100 pcs - 0.20 USD다음의 수량에 대한 총 가격 100 pcs - 0.20 USD
다음의 수량에 대한 순 가격 200 pcs - 0.18 USD다음의 수량에 대한 총 가격 200 pcs - 0.18 USD
다음의 수량에 대한 순 가격 600 pcs - 0.16 USD다음의 수량에 대한 총 가격 600 pcs - 0.16 USD
다음의 수량에 대한 순 가격 1000 pcs - 0.15 USD다음의 수량에 대한 총 가격 1000 pcs - 0.15 USD
다음의 수량에 대한 순 가격 2600 pcs - 0.14 USD다음의 수량에 대한 총 가격 2600 pcs - 0.14 USD
다음의 수량에 대한 순 가격 5000 pcs - 0.14 USD다음의 수량에 대한 총 가격 5000 pcs - 0.14 USD
3737 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
TAJB106K016RNJ | 커패시터: 탄탈륨; 10uF; 16VDC; SMD; B; 1411; ±10%; -55÷125°C; TAJ; 180mm
커패시터: 탄탈륨; 10uF; 16VDC; SMD; B; 1411; ±10%; -55÷125°C; TAJ; 180mm
제조업체 부품 번호: TAJB106K016RNJ
제조사: KYOCERA AVX
다음의 수량에 대한 순 가격 1 pcs - 0.68 USD다음의 수량에 대한 총 가격 1 pcs - 0.68 USD
다음의 수량에 대한 순 가격 10 pcs - 0.38 USD다음의 수량에 대한 총 가격 10 pcs - 0.38 USD
다음의 수량에 대한 순 가격 50 pcs - 0.24 USD다음의 수량에 대한 총 가격 50 pcs - 0.24 USD
다음의 수량에 대한 순 가격 100 pcs - 0.20 USD다음의 수량에 대한 총 가격 100 pcs - 0.20 USD
다음의 수량에 대한 순 가격 500 pcs - 0.15 USD다음의 수량에 대한 총 가격 500 pcs - 0.15 USD
다음의 수량에 대한 순 가격 1000 pcs - 0.13 USD다음의 수량에 대한 총 가격 1000 pcs - 0.13 USD
다음의 수량에 대한 순 가격 2000 pcs - 0.13 USD다음의 수량에 대한 총 가격 2000 pcs - 0.13 USD
다음의 수량에 대한 순 가격 4000 pcs - 0.12 USD다음의 수량에 대한 총 가격 4000 pcs - 0.12 USD
다음의 수량에 대한 순 가격 6000 pcs - 0.12 USD다음의 수량에 대한 총 가격 6000 pcs - 0.12 USD
다음의 수량에 대한 순 가격 10000 pcs - 0.12 USD다음의 수량에 대한 총 가격 10000 pcs - 0.12 USD
10726 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
거의 사용할 수 없는 제품
CC-104/100 | 커패시터: 세라믹; 100nF; 100V; Y5V; -20÷80%; THT; 5mm
커패시터: 세라믹; 100nF; 100V; Y5V; -20÷80%; THT; 5mm
제조업체 부품 번호: CC-104/100
제조사: SR PASSIVES
다음의 수량에 대한 순 가격 100 pcs - 0.04 USD다음의 수량에 대한 총 가격 100 pcs - 0.04 USD
다음의 수량에 대한 순 가격 1000 pcs - 0.02 USD다음의 수량에 대한 총 가격 1000 pcs - 0.02 USD
다음의 수량에 대한 순 가격 5000 pcs - 0.02 USD다음의 수량에 대한 총 가격 5000 pcs - 0.02 USD
36000 TME에 재고 있음
개 번호 (다양성: 100)
최소 주문 수량: 100.
다수: 100.
UES1E470MPM | 커패시터: 전해질; 양극; THT; 47uF; 25VDC; Ø10x12.5mm; 피치: 5mm; ±20%; 1000h
커패시터: 전해질; 양극; THT; 47uF; 25VDC; Ø10x12.5mm; 피치: 5mm; ±20%; 1000h
제조업체 부품 번호: UES1E470MPM
제조사: NICHICON
다음의 수량에 대한 순 가격 1 pcs - 0.74 USD다음의 수량에 대한 총 가격 1 pcs - 0.74 USD
다음의 수량에 대한 순 가격 10 pcs - 0.41 USD다음의 수량에 대한 총 가격 10 pcs - 0.41 USD
다음의 수량에 대한 순 가격 50 pcs - 0.35 USD다음의 수량에 대한 총 가격 50 pcs - 0.35 USD
다음의 수량에 대한 순 가격 100 pcs - 0.32 USD다음의 수량에 대한 총 가격 100 pcs - 0.32 USD
다음의 수량에 대한 순 가격 200 pcs - 0.30 USD다음의 수량에 대한 총 가격 200 pcs - 0.30 USD
다음의 수량에 대한 순 가격 600 pcs - 0.27 USD다음의 수량에 대한 총 가격 600 pcs - 0.27 USD
다음의 수량에 대한 순 가격 1000 pcs - 0.26 USD다음의 수량에 대한 총 가격 1000 pcs - 0.26 USD
다음의 수량에 대한 순 가격 2600 pcs - 0.23 USD다음의 수량에 대한 총 가격 2600 pcs - 0.23 USD
다음의 수량에 대한 순 가격 5000 pcs - 0.23 USD다음의 수량에 대한 총 가격 5000 pcs - 0.23 USD
1070 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
293D106X9010A2TE3 | 커패시터: 탄탈륨; 10uF; 10VDC; SMD; A; 1206; ±10%; -55÷125°C; Tantamount
커패시터: 탄탈륨; 10uF; 10VDC; SMD; A; 1206; ±10%; -55÷125°C; Tantamount
제조업체 부품 번호: 293D106X9010A2TE3
제조사: VISHAY
다음의 수량에 대한 순 가격 1 pcs - 0.20 USD다음의 수량에 대한 총 가격 1 pcs - 0.20 USD
다음의 수량에 대한 순 가격 10 pcs - 0.16 USD다음의 수량에 대한 총 가격 10 pcs - 0.16 USD
다음의 수량에 대한 순 가격 50 pcs - 0.13 USD다음의 수량에 대한 총 가격 50 pcs - 0.13 USD
다음의 수량에 대한 순 가격 100 pcs - 0.11 USD다음의 수량에 대한 총 가격 100 pcs - 0.11 USD
다음의 수량에 대한 순 가격 500 pcs - 0.08 USD다음의 수량에 대한 총 가격 500 pcs - 0.08 USD
다음의 수량에 대한 순 가격 1000 pcs - 0.07 USD다음의 수량에 대한 총 가격 1000 pcs - 0.07 USD
다음의 수량에 대한 순 가격 2000 pcs - 0.07 USD다음의 수량에 대한 총 가격 2000 pcs - 0.07 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
EWH1EV101E11OT | 커패시터: 전해질; THT; 100uF; 25VDC; Ø6.3x11mm; 피치: 2.5mm; ±20%; 2000h
커패시터: 전해질; THT; 100uF; 25VDC; Ø6.3x11mm; 피치: 2.5mm; ±20%; 2000h
제조업체 부품 번호: EWH1EV101E11OT
제조사: AISHI
다음의 수량에 대한 순 가격 20 pcs - 0.07 USD다음의 수량에 대한 총 가격 20 pcs - 0.07 USD
다음의 수량에 대한 순 가격 100 pcs - 0.03 USD다음의 수량에 대한 총 가격 100 pcs - 0.03 USD
다음의 수량에 대한 순 가격 500 pcs - 0.02 USD다음의 수량에 대한 총 가격 500 pcs - 0.02 USD
다음의 수량에 대한 순 가격 1000 pcs - 0.02 USD다음의 수량에 대한 총 가격 1000 pcs - 0.02 USD
다음의 수량에 대한 순 가격 5000 pcs - 0.02 USD다음의 수량에 대한 총 가격 5000 pcs - 0.02 USD
73680 TME에 재고 있음
개 번호 (다양성: 10)
최소 주문 수량: 20.
다수: 10.
EWH1VM471G16OT | 커패시터: 전해질; THT; 470uF; 35VDC; Ø10x16mm; 피치: 5mm; ±20%; 2000h; H: 16mm
커패시터: 전해질; THT; 470uF; 35VDC; Ø10x16mm; 피치: 5mm; ±20%; 2000h; H: 16mm
제조업체 부품 번호: EWH1VM471G16OT
제조사: AISHI
다음의 수량에 대한 순 가격 10 pcs - 0.19 USD다음의 수량에 대한 총 가격 10 pcs - 0.19 USD
다음의 수량에 대한 순 가격 100 pcs - 0.08 USD다음의 수량에 대한 총 가격 100 pcs - 0.08 USD
다음의 수량에 대한 순 가격 250 pcs - 0.07 USD다음의 수량에 대한 총 가격 250 pcs - 0.07 USD
다음의 수량에 대한 순 가격 500 pcs - 0.06 USD다음의 수량에 대한 총 가격 500 pcs - 0.06 USD
다음의 수량에 대한 순 가격 1000 pcs - 0.06 USD다음의 수량에 대한 총 가격 1000 pcs - 0.06 USD
다음의 수량에 대한 순 가격 2500 pcs - 0.06 USD다음의 수량에 대한 총 가격 2500 pcs - 0.06 USD
다음의 수량에 대한 순 가격 5000 pcs - 0.06 USD다음의 수량에 대한 총 가격 5000 pcs - 0.06 USD
다음의 수량에 대한 순 가격 10000 pcs - 0.06 USD다음의 수량에 대한 총 가격 10000 pcs - 0.06 USD
다음의 수량에 대한 순 가격 20000 pcs - 0.06 USD다음의 수량에 대한 총 가격 20000 pcs - 0.06 USD
78620 TME에 재고 있음
개 번호 (다양성: 10)
최소 주문 수량: 10.
다수: 10.
MKS2C041001F00KSSD | 커패시터: 폴리에스테르; 1uF; 40VAC; 63VDC; 5mm; ±10%; 5x10x7.2mm; MKT; THT
커패시터: 폴리에스테르; 1uF; 40VAC; 63VDC; 5mm; ±10%; 5x10x7.2mm; MKT; THT
제조업체 부품 번호: MKS2C041001F00KSSD
제조사: WIMA
다음의 수량에 대한 순 가격 1 pcs - 0.99 USD다음의 수량에 대한 총 가격 1 pcs - 0.99 USD
다음의 수량에 대한 순 가격 10 pcs - 0.63 USD다음의 수량에 대한 총 가격 10 pcs - 0.63 USD
다음의 수량에 대한 순 가격 50 pcs - 0.50 USD다음의 수량에 대한 총 가격 50 pcs - 0.50 USD
다음의 수량에 대한 순 가격 100 pcs - 0.45 USD다음의 수량에 대한 총 가격 100 pcs - 0.45 USD
다음의 수량에 대한 순 가격 250 pcs - 0.40 USD다음의 수량에 대한 총 가격 250 pcs - 0.40 USD
다음의 수량에 대한 순 가격 500 pcs - 0.36 USD다음의 수량에 대한 총 가격 500 pcs - 0.36 USD
다음의 수량에 대한 순 가격 1000 pcs - 0.33 USD다음의 수량에 대한 총 가격 1000 pcs - 0.33 USD
다음의 수량에 대한 순 가격 3500 pcs - 0.30 USD다음의 수량에 대한 총 가격 3500 pcs - 0.30 USD
다음의 수량에 대한 순 가격 7000 pcs - 0.30 USD다음의 수량에 대한 총 가격 7000 pcs - 0.30 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
거의 사용할 수 없는 제품
MKP-X2-100NR15/310 | 커패시터: 폴리프로필렌; X2; 100nF; 310VAC; 18x12x6mm; THT; ±10%; 15mm
커패시터: 폴리프로필렌; X2; 100nF; 310VAC; 18x12x6mm; THT; ±10%; 15mm
제조업체 부품 번호: MKP-X2-100NR15/310
제조사: SR PASSIVES
다음의 수량에 대한 순 가격 10 pcs - 0.09 USD다음의 수량에 대한 총 가격 10 pcs - 0.09 USD
다음의 수량에 대한 순 가격 100 pcs - 0.05 USD다음의 수량에 대한 총 가격 100 pcs - 0.05 USD
다음의 수량에 대한 순 가격 500 pcs - 0.04 USD다음의 수량에 대한 총 가격 500 pcs - 0.04 USD
다음의 수량에 대한 순 가격 1000 pcs - 0.04 USD다음의 수량에 대한 총 가격 1000 pcs - 0.04 USD
다음의 수량에 대한 순 가격 2000 pcs - 0.03 USD다음의 수량에 대한 총 가격 2000 pcs - 0.03 USD
다음의 수량에 대한 순 가격 5000 pcs - 0.03 USD다음의 수량에 대한 총 가격 5000 pcs - 0.03 USD
다음의 수량에 대한 순 가격 10000 pcs - 0.03 USD다음의 수량에 대한 총 가격 10000 pcs - 0.03 USD
다음의 수량에 대한 순 가격 20000 pcs - 0.03 USD다음의 수량에 대한 총 가격 20000 pcs - 0.03 USD
16507 TME에 재고 있음
개 번호 (다양성: 10)
최소 주문 수량: 10.
다수: 10.
K104K10X7RF5UL2 | 커패시터: 세라믹; 100nF; 50V; X7R; ±10%; THT; 2.5mm
커패시터: 세라믹; 100nF; 50V; X7R; ±10%; THT; 2.5mm
제조업체 부품 번호: K104K10X7RF5UL2
제조사: VISHAY
다음의 수량에 대한 순 가격 1 pcs - 0.23 USD다음의 수량에 대한 총 가격 1 pcs - 0.23 USD
다음의 수량에 대한 순 가격 10 pcs - 0.14 USD다음의 수량에 대한 총 가격 10 pcs - 0.14 USD
다음의 수량에 대한 순 가격 100 pcs - 0.09 USD다음의 수량에 대한 총 가격 100 pcs - 0.09 USD
다음의 수량에 대한 순 가격 500 pcs - 0.07 USD다음의 수량에 대한 총 가격 500 pcs - 0.07 USD
다음의 수량에 대한 순 가격 1000 pcs - 0.06 USD다음의 수량에 대한 총 가격 1000 pcs - 0.06 USD
다음의 수량에 대한 순 가격 2500 pcs - 0.06 USD다음의 수량에 대한 총 가격 2500 pcs - 0.06 USD
다음의 수량에 대한 순 가격 5000 pcs - 0.05 USD다음의 수량에 대한 총 가격 5000 pcs - 0.05 USD
다음의 수량에 대한 순 가격 10000 pcs - 0.05 USD다음의 수량에 대한 총 가격 10000 pcs - 0.05 USD
다음의 수량에 대한 순 가격 20000 pcs - 0.05 USD다음의 수량에 대한 총 가격 20000 pcs - 0.05 USD
8350 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
R82DC3100DQ50K | 커패시터: 폴리에스테르; 100nF; 40VAC; 63VDC; 5mm; ±10%; 2.5x6.5x7.2mm; R82; THT
커패시터: 폴리에스테르; 100nF; 40VAC; 63VDC; 5mm; ±10%; 2.5x6.5x7.2mm; R82; THT
제조업체 부품 번호: R82DC3100DQ50K
제조사: KEMET
다음의 수량에 대한 순 가격 1 pcs - 0.36 USD다음의 수량에 대한 총 가격 1 pcs - 0.36 USD
다음의 수량에 대한 순 가격 10 pcs - 0.15 USD다음의 수량에 대한 총 가격 10 pcs - 0.15 USD
다음의 수량에 대한 순 가격 50 pcs - 0.13 USD다음의 수량에 대한 총 가격 50 pcs - 0.13 USD
다음의 수량에 대한 순 가격 100 pcs - 0.12 USD다음의 수량에 대한 총 가격 100 pcs - 0.12 USD
다음의 수량에 대한 순 가격 500 pcs - 0.10 USD다음의 수량에 대한 총 가격 500 pcs - 0.10 USD
다음의 수량에 대한 순 가격 1000 pcs - 0.09 USD다음의 수량에 대한 총 가격 1000 pcs - 0.09 USD
다음의 수량에 대한 순 가격 3500 pcs - 0.08 USD다음의 수량에 대한 총 가격 3500 pcs - 0.08 USD
다음의 수량에 대한 순 가격 7000 pcs - 0.07 USD다음의 수량에 대한 총 가격 7000 pcs - 0.07 USD
다음의 수량에 대한 순 가격 10500 pcs - 0.07 USD다음의 수량에 대한 총 가격 10500 pcs - 0.07 USD
다음의 수량에 대한 순 가격 21000 pcs - 0.06 USD다음의 수량에 대한 총 가격 21000 pcs - 0.06 USD
35302 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
TAJA106K010RNJ | 커패시터: 탄탈륨; 10uF; 10VDC; SMD; A; 1206; ±10%; -55÷125°C; TAJ; 180mm
커패시터: 탄탈륨; 10uF; 10VDC; SMD; A; 1206; ±10%; -55÷125°C; TAJ; 180mm
제조업체 부품 번호: TAJA106K010RNJ
제조사: KYOCERA AVX
다음의 수량에 대한 순 가격 1 pcs - 0.74 USD다음의 수량에 대한 총 가격 1 pcs - 0.74 USD
다음의 수량에 대한 순 가격 10 pcs - 0.36 USD다음의 수량에 대한 총 가격 10 pcs - 0.36 USD
다음의 수량에 대한 순 가격 100 pcs - 0.20 USD다음의 수량에 대한 총 가격 100 pcs - 0.20 USD
다음의 수량에 대한 순 가격 500 pcs - 0.13 USD다음의 수량에 대한 총 가격 500 pcs - 0.13 USD
다음의 수량에 대한 순 가격 1000 pcs - 0.11 USD다음의 수량에 대한 총 가격 1000 pcs - 0.11 USD
다음의 수량에 대한 순 가격 2000 pcs - 0.10 USD다음의 수량에 대한 총 가격 2000 pcs - 0.10 USD
다음의 수량에 대한 순 가격 4000 pcs - 0.09 USD다음의 수량에 대한 총 가격 4000 pcs - 0.09 USD
다음의 수량에 대한 순 가격 6000 pcs - 0.09 USD다음의 수량에 대한 총 가격 6000 pcs - 0.09 USD
다음의 수량에 대한 순 가격 10000 pcs - 0.09 USD다음의 수량에 대한 총 가격 10000 pcs - 0.09 USD
다음의 수량에 대한 순 가격 20000 pcs - 0.09 USD다음의 수량에 대한 총 가격 20000 pcs - 0.09 USD
63706 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
거의 사용할 수 없는 제품
표준 오퍼에 포함되지 않은 제품에 대한 요청
요청이 성공적으로 전송되었습니다. 곧 제공된 이메일 주소로 제품 구매 제안서를 보내드리겠습니다.
고객 번호
제조업체 부품 번호
제조 업체
총액
이메일주소
메시지 내용