+1500000 개 이상의 제품 제공
하루에 7000개의 패키지
150개국에서 28만 명 이상의 고객
Classic car antenna system, consisting of an antenna on the roof of the vehicle, coaxial cable ended with a DIN connector, and a radio receiver, is becoming increasingly rare. Development of the automotive industry made manufacturers to develop own connectivity solutions. Car antenna plugs and adapters allow to attach different standard antennas to existing factory radio receivers. They also allow to attach factory antennas to a different radio receiver (e.g. a radio with a navigation system) and distribute signal among two devices.
Adapters are so diverse that they can be used for all antenna connector combinations available in the market, such as: DIN sockets and plugs, ISO connectors, Fakra circular connectors, RAKU, RAKU II, and FME connectors, Snap straight and angled connectors as well as versions with both plugs and sockets. Thera are also variants with a round connector and an bolt nuts with metric thread, and one-sided connectors, having a connector on the one side, and a cable on the other. Such solutions are commonly called pigtail connectors.
Adapters vary in cable length and workmanship. Thanks to this fact it is easier to match them to existing vehicle’s interior, e.g. its ceiling lining. There are also compact adapters designed to be mounted directly in the receiver’s socket; they come without any cables.
Apart from adapters, in TME’s offer there are also extension cables for antennas and antenna separators. They can be used for both leading power and signal to an amplifier placed in an antenna socket.
A lot of adapters are, however, adjusted to specific vehicle brands. Thanks to this fact it is easier to choose the one that we need. Our customers can find accessories that suit their specific needs by using our search engine, sections containing lists of parameters, located above product list, or product comparison engine where it is possible to view available assortment and choose the appropriate product that meets selected criteria.
창고: