+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

카테고리를 찾을 수 없음

(0)

The Global Positioning System (GPS) is commonly used all over the world. It provides location data and facilitates navigation. It is used in automotive and aerospace industries, in portable multimedia devices, or industrial machinery. There is a wide range of GPS antennas on the market, which makes it possible to implement this system in particular applications. Due to technology development, it is now possible to manufacture ceramic antennas of very compact dimensions, as small as several millimeters. High effectiveness is achieved with low power consumption, which is a crucial factor in numerous projects. Modern GPS antennas ensure high sensitivity and resistance to environmental conditions, such as dust, high temperatures, or high level of humidity.

GPS antennas in TME’s offer

In its offer TME has a wide range of GPS antennas with different parameters. Ceramic antennas of compact dimensions come handy in systems with strict space limitations. The catalogue also includes the so-called combo antennas, which cover a wide range of frequencies and protocols (e.g. GPS, GSM, and WiFi) in a single device. Despite their compact form, they offer high sensitivity, long range, and resistance to external factors. Search filters allow you to narrow down the product list by operating temperature, supported protocols, type of connector, power consumption, or antenna gain. The last parameter describes the amount of decibels, by which the gain of a particular antenna is higher than that of a reference antenna (while providing the same amount of power). Transfer Multisort Elektronik distributes well-proven products from such manufacturers as Molex, OriginGPS, or SR Passives.

선택한 카테고리의 제품을 찾을 수 없습니다. TME 제안을 추천합니다:확인
표준 오퍼에 포함되지 않은 제품에 대한 요청
요청이 성공적으로 전송되었습니다. 곧 제공된 이메일 주소로 제품 구매 제안서를 보내드리겠습니다.
고객 번호
제조업체 부품 번호
제조 업체
총액
이메일주소
메시지 내용