+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

카테고리를 찾을 수 없음

(0)

A magnet is an object that generates a magnetic field. The most important feature of this type of material is the force of attraction of ferromagnets, such as iron. Magnets react to each other – attracting or repelling one another, depending on the location of the pole. Permanent magnets can be divided according to the material used: neodymium magnets (a combination of neodymium, iron and boron), samarium-cobalt, ceramic, ferrite or plastic magnets are used in industry They are used in the production of household appliances, computer components, filtration systems, electric motors, compasses, meters and various fixtures. When choosing an appropriate magnet, it’s worth paying attention to the force that defines how strong the attraction will be. In many cases, additional fastening may also be crucial – manufacturers place mounting holes in their magnets, as well as external and internal threads.

Magnets available at TME

TME offers sensors and transducers, including magnets of different shapes, forces and types. Our product catalogue includes both neodymium and samarium-cobalt magnets as well as those made of hard ferrite. The offer includes magnets with force ranging from 2.5N to 1.1kN. Transfer Multisort Elektronik distributes standard round magnets as well as versions with through-holes and threads (external and internal). Some of them have plastic or steel enclosures. Each product contains a catalogue sheet with overall dimensions and mounting method, as well as information about the price and availability. TME offers components of such manufacturers as Elesa+Ganter, Assemtech and Omron.

선택한 카테고리의 제품을 찾을 수 없습니다. TME 제안을 추천합니다:확인
표준 오퍼에 포함되지 않은 제품에 대한 요청
요청이 성공적으로 전송되었습니다. 곧 제공된 이메일 주소로 제품 구매 제안서를 보내드리겠습니다.
고객 번호
제조업체 부품 번호
제조 업체
총액
이메일주소
메시지 내용