+1500000 개 이상의 제품 제공
하루에 6000개의 패키지
150개국에서 28만 명 이상의 고객
2026년 07월12일 오후 08시 00분 - 11시 00분 (CEST) 웹사이트 접속 및 온라인 주문에 문제가 발생할 수 있음을 알려드립니다. 불편을 끼쳐 드려 죄송합니다.
For many machines and devices a stable working position is very important. In the case of large mobile equipment, it’s important that the wheels used are resistant to heavy loads and make it easier to move the machine. Therefore, it’s worthwhile to ensure that levelling feet and wheels are properly matched to the parameters of the device. With a wide range of manufacturers, you can select elements for different applications. For machines operating in dirty areas, use transport wheels and levelling feet resistant to oils, solvents, greases or acids. This will increase their service life. In addition, you can use suitable construction materials to reduce vibrations. This has a positive effect on the durability of the machines and also increases the safety of the equipment by reducing the risk of uncontrolled change of position. Additionally, wheels and levelling feet made of such materials reduce the noise in the immediate vicinity of the machines. Properly selected plastic materials also help protect the flooring.
Transfer Multisort Elektronik offers levelling feet, wheels, legs and accessories useful during their assembly and use. Making a choice is easier thanks to an extensive system of search engine filters. Components can be selected according to the type and version of the element, materials used in its construction and dimensions. The parameters referring to load resistance will also be very useful – i.e. load capacity (products that hold from several dozen kilograms to even a few tons are available), static and dynamic loads (expressed in N), rolling load capacity, as well as its Shore hardness. TME offers this category of products from many renowned manufacturers specializing in the production of mechanical elements of this kind, i.e.: Elesa+Ganter, Fix&Fasten, Colson and FATH.
창고: