+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

거리 센서

(129)

Distance sensors are electronic components that are commonly used in many industries. First of all, they are used in industrial automation and robotics, but we often encounter them in everyday life as well. Many devices and machines, such as cars and elevators, contain distance sensors that make it possible to implement safety features and functions, such as a parking assistant or adaptive cruise control. In industrial conditions, distance sensors allow to detect the position of an object on the production/transmission line, position the object placed in the machine, determine its size, etc. Constructors and designers select the appropriate type of component strictly depending on the characteristics of the application, required accuracy, operating speed and the system in which the sensor will perform its role. Let us take a look at the basic parameters of sensors that should be considered when looking for the right solution.

How distance sensors work – technology and classification

Distance sensors most often consist of three elements: a controller, an emitter and a receiver. The controller uses the transmitter to send a signal (acoustic, electromagnetic) and then "waits" for the wave to bounce off the nearest surface and be registered by the receiver. The measurement can be made in two ways. (1) Given the time and speed of wave propagation, the controller calculates the distance travelled by the signal, and then sends this information to the master device. (2) Another method is to register the intensity of the reflected light (the weaker the returning wave, the greater the distance the sensor registers). The basic division of sensors is based on the type of the emitted signal.

Laser distance sensor

The undoubted advantage of laser sensors is their accuracy and range: the emitted beam is sent to a precisely defined point, and its appropriate propagation allows for the detection of objects located at a distance of even several dozen meters. At the same time, sampling can be performed with a frequency of several hundred hertz. In projects where the price of the component does not play a key role, a laser distance sensor will usually be the best possible solution.

Infrared and reflective distance sensors

“Reflective” sensors have a somewhat misleading name because, as described above, distance detection is usually done by reflecting some type of a signal. Elements of these type use IR (i.e. infrared) emitting diodes and a detector, e.g. a phototransistor. Compared to a laser beam, the signal is weaker and scattered. On the one hand, it limits the precision of the measurement and its maximum distance, and on the other hand, it allows the construction of sensors that detect objects present in a much wider field (they can be conventionally called the "sensor's field of view"). These types of sensors are used, among others as "cliff sensors" that prevent the machine from falling – this role is found, for example, in automatic vacuum cleaners. The range and precision are improved by using a series of sensor arrays in a single module. Equipped with many outputs, the circuit allows, for example, to detect movement parallel to the sensor plane (speed measurement). It should be noted here that the reflection sensors that record the intensity of the returning signal are perfect for detecting dark, light-absorbing surfaces. They are therefore used for detecting printed lines or counting pulses in encoders that control the speed of rotation and axis position (slot sensors).

Ultrasonic distance sensor

Ultrasonic sensors, unlike the photodetectors described above, use the propagation of acoustic waves. This solution has several advantages. First of all, the sensor can detect objects made of transparent materials as well as liquids. An example of a daily use is the circuit monitoring the water level in the tank. As the piezoelectric emitter vibrates, a (desirable) side effect of its operation is cleaning the sensor, especially of dust and tarnish. In the case of a laser sensor, similar contamination could lead to erroneous readings. Ultrasonic sensors are easy to implement and affordable, making them popular among amateur builders, especially in the construction of self-propelled robots (obstacle detection).

Distance sensor interface

Another key issue to consider when choosing a distance sensor is the type of interface. The basic division is, of course, the division into analogue and digital interfaces.

Analogue interface

Thanks to the analogue interface (current or voltage), the control system (e.g. a microcontroller) has direct access to the sensor readings and can analyze, correct, calibrate and compensate the measurement against environmental factors. It also facilitates software calibration of the sensor. Moreover, the constructor can use the analogue signal to generate interrupts, so exceeding the set value will result in an immediate reaction of the control system. The most common application of analogue interfaces is in the case of reflection sensors – the interface can be, for example, a phototransistor collector.

Digital interface

The undoubted advantage of digital interfaces is their resistance to electromagnetic radiation and the limitation of the number of wires required. In the case of the analogue interface, each sensor takes one line of the controller (or multiplexer, A/C converter). The use of such a transmission method as, for example, I2C allows (theoretically) to connect literally hundreds of sensors to one line. Digital interfaces are a desirable solution in industrial settings, as they allow easy integration with existing control systems.

제품: 129

창고:

TME
전부
페이지 1
SEN0311 | 감지기: 거리; 초음파; 3.3÷5VDC; UART; 0.03÷4.5m; 기능: 방수
감지기: 거리; 초음파; 3.3÷5VDC; UART; 0.03÷4.5m; 기능: 방수
제조업체 부품 번호: SEN0311
제조사: DFROBOT
다음의 수량에 대한 순 가격 1 pcs - 23.35 USD다음의 수량에 대한 총 가격 1 pcs - 23.35 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
VL53L1X TIME-OF-FLIGHT DISTANCE SENSOR | 감지기: 거리; 레이저; 2.6÷5.5VDC; I2C; 거리 범위: 0.04÷4m; IC: VL53L1X; 해상도: 1mm
감지기: 거리; 레이저; 2.6÷5.5VDC; I2C; 거리 범위: 0.04÷4m; IC: VL53L1X; 해상도: 1mm
제조업체 부품 번호: VL53L1X TIME-OF-FLIGHT DISTANCE SENSOR
제조사: POLOLU
중요한 정보: 주의! 레이저 방사선! 안전 지침을 준수하십시오. 레이저 광원을 직접 응시하지 마십시오.
다음의 수량에 대한 순 가격 1 pcs - 23.90 USD다음의 수량에 대한 총 가격 1 pcs - 23.90 USD
다음의 수량에 대한 순 가격 3 pcs - 21.11 USD다음의 수량에 대한 총 가격 3 pcs - 21.11 USD
15 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
ULTRASONIC RANGER | 감지기: 거리; 초음파; 3.2÷5.2VDC; Grove Interface (4-wire),PWM; Ch: 1; 나사
감지기: 거리; 초음파; 3.2÷5.2VDC; Grove Interface (4-wire),PWM; Ch: 1; 나사
제조업체 부품 번호: ULTRASONIC RANGER
제조사: SEEED STUDIO
다음의 수량에 대한 순 가격 1 pcs - 4.37 USD다음의 수량에 대한 총 가격 1 pcs - 4.37 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
QTR-8RC REFLECTANCE SENSOR ARRAY | 감지기: 거리; 반사식; 3.3÷5VDC; Ch: 8; 75x12.7mm; 디지털 출력: 8; 구성 요소: KTIR0711S
감지기: 거리; 반사식; 3.3÷5VDC; Ch: 8; 75x12.7mm; 디지털 출력: 8; 구성 요소: KTIR0711S
제조업체 부품 번호: QTR-8RC REFLECTANCE SENSOR ARRAY
제조사: POLOLU
다음의 수량에 대한 순 가격 1 pcs - 14.44 USD다음의 수량에 대한 총 가격 1 pcs - 14.44 USD
다음의 수량에 대한 순 가격 3 pcs - 12.75 USD다음의 수량에 대한 총 가격 3 pcs - 12.75 USD
1 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
SEN0592 | 감지기: 거리; 초음파; 3.3÷24VDC; RS485; 0.03÷5m; -30÷80°C; 10mA; IP67
감지기: 거리; 초음파; 3.3÷24VDC; RS485; 0.03÷5m; -30÷80°C; 10mA; IP67
제조업체 부품 번호: SEN0592
제조사: DFROBOT
다음의 수량에 대한 순 가격 1 pcs - 35.05 USD다음의 수량에 대한 총 가격 1 pcs - 35.05 USD
다음의 수량에 대한 순 가격 5 pcs - 31.77 USD다음의 수량에 대한 총 가격 5 pcs - 31.77 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
SEN0164 | 감지기: 거리; 적외선; 5VDC; 숫자의; Ch: 1; 전부: 모듈,케이블; Gravity; 범위: 3÷50cm; Arduino
감지기: 거리; 적외선; 5VDC; 숫자의; Ch: 1; 전부: 모듈,케이블; Gravity; 범위: 3÷50cm; Arduino
제조업체 부품 번호: SEN0164
제조사: DFROBOT
다음의 수량에 대한 순 가격 1 pcs - 7.33 USD다음의 수량에 대한 총 가격 1 pcs - 7.33 USD
30 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
VL53L0X TIME-OF-FLIGHT DISTANCE SENSOR | 감지기: 거리; 적외선; 2.6÷5.5VDC; I2C; 30÷2000mm; IC: VL53L0X
감지기: 거리; 적외선; 2.6÷5.5VDC; I2C; 30÷2000mm; IC: VL53L0X
제조업체 부품 번호: VL53L0X TIME-OF-FLIGHT DISTANCE SENSOR
제조사: POLOLU
다음의 수량에 대한 순 가격 1 pcs - 20.81 USD다음의 수량에 대한 총 가격 1 pcs - 20.81 USD
다음의 수량에 대한 순 가격 3 pcs - 18.32 USD다음의 수량에 대한 총 가격 3 pcs - 18.32 USD
5 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
SEN0245 | 감지기: 거리; 레이저,time-of-flight (ToF); 3.3÷5VDC; I2C; 거리 범위: 0.03÷2m
감지기: 거리; 레이저,time-of-flight (ToF); 3.3÷5VDC; I2C; 거리 범위: 0.03÷2m
제조업체 부품 번호: SEN0245
제조사: DFROBOT
중요한 정보: 주의! 레이저 방사선! 안전 지침을 준수하십시오. 레이저 광원을 직접 응시하지 마십시오.
다음의 수량에 대한 순 가격 1 pcs - 13.07 USD다음의 수량에 대한 총 가격 1 pcs - 13.07 USD
7 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
SEN0307 | 감지기: 거리; 초음파; 3.3÷5.5VDC; 거리 범위: 0.02÷5m; 치수: 47x22mm; 해상도: 10mm
감지기: 거리; 초음파; 3.3÷5.5VDC; 거리 범위: 0.02÷5m; 치수: 47x22mm; 해상도: 10mm
제조업체 부품 번호: SEN0307
제조사: DFROBOT
다음의 수량에 대한 순 가격 1 pcs - 8.51 USD다음의 수량에 대한 총 가격 1 pcs - 8.51 USD
6 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
SEN0019 | 감지기: 거리; 적외선; 5VDC; 아날로그식의; Ch: 1; 30÷800mm; 전부: 모듈,케이블; Gravity
감지기: 거리; 적외선; 5VDC; 아날로그식의; Ch: 1; 30÷800mm; 전부: 모듈,케이블; Gravity
제조업체 부품 번호: SEN0019
제조사: DFROBOT
다음의 수량에 대한 순 가격 1 pcs - 7.93 USD다음의 수량에 대한 총 가격 1 pcs - 7.93 USD
2 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
38 KHZ IR PROXIMITY SENSOR LOW BRIGHTNES | 감지기: 거리; 적외선; 3.3÷5VDC; 아날로그식의; 0÷300mm; 1kHz; IC: TSSP77038
감지기: 거리; 적외선; 3.3÷5VDC; 아날로그식의; 0÷300mm; 1kHz; IC: TSSP77038
제조업체 부품 번호: 38 KHZ IR PROXIMITY SENSOR LOW BRIGHTNES
제조사: POLOLU
다음의 수량에 대한 순 가격 1 pcs - 10.76 USD다음의 수량에 대한 총 가격 1 pcs - 10.76 USD
다음의 수량에 대한 순 가격 3 pcs - 9.46 USD다음의 수량에 대한 총 가격 3 pcs - 9.46 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
SEN0259 | 감지기: 거리; 레이저,LIDAR,time-of-flight (ToF); 4.5÷6VDC; I2C,UART; 2°
감지기: 거리; 레이저,LIDAR,time-of-flight (ToF); 4.5÷6VDC; I2C,UART; 2°
제조업체 부품 번호: SEN0259
제조사: DFROBOT
중요한 정보: 주의! 레이저 방사선! 안전 지침을 준수하십시오. 레이저 광원을 직접 응시하지 마십시오.
다음의 수량에 대한 순 가격 1 pcs - 52.95 USD다음의 수량에 대한 총 가격 1 pcs - 52.95 USD
1 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
QTR-1A REFLECTANCE SENSOR | 감지기: 거리; 반사식; 5VDC; 아날로그식의; Ch: 1; 7.6x12.7mm; 아날로그 출력: 1; 2개
감지기: 거리; 반사식; 5VDC; 아날로그식의; Ch: 1; 7.6x12.7mm; 아날로그 출력: 1; 2개
제조업체 부품 번호: QTR-1A REFLECTANCE SENSOR
제조사: POLOLU
다음의 수량에 대한 순 가격 1 set - 6.27 USD다음의 수량에 대한 총 가격 1 set - 6.27 USD
다음의 수량에 대한 순 가격 3 set - 5.53 USD다음의 수량에 대한 총 가격 3 set - 5.53 USD
0 TME에 재고 있음
완전한 세트 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
SEN0208 | 감지기: 거리; 초음파; 5VDC; 0.25÷4.5m
감지기: 거리; 초음파; 5VDC; 0.25÷4.5m
제조업체 부품 번호: SEN0208
제조사: DFROBOT
다음의 수량에 대한 순 가격 1 pcs - 15.07 USD다음의 수량에 대한 총 가격 1 pcs - 15.07 USD
6 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
4064 | 감지기: 거리; 거리 범위: 1÷500mm; 치수: 21.6x8.9x3.5mm; 15°; 출력 신호: 디지털(0 또는 1)
감지기: 거리; 거리 범위: 1÷500mm; 치수: 21.6x8.9x3.5mm; 15°; 출력 신호: 디지털(0 또는 1)
제조업체 부품 번호: 4064
제조사: POLOLU
다음의 수량에 대한 순 가격 1 pcs - 22.21 USD다음의 수량에 대한 총 가격 1 pcs - 22.21 USD
다음의 수량에 대한 순 가격 3 pcs - 19.62 USD다음의 수량에 대한 총 가격 3 pcs - 19.62 USD
10 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
QTRX-MD-08A REFLECTANCE SENSOR ARRAY | 감지기: 거리; 반사식; 2.9÷5.5VDC; 아날로그식의; Ch: 8; 61x20mm; MD
감지기: 거리; 반사식; 2.9÷5.5VDC; 아날로그식의; Ch: 8; 61x20mm; MD
제조업체 부품 번호: QTRX-MD-08A REFLECTANCE SENSOR ARRAY
제조사: POLOLU
다음의 수량에 대한 순 가격 1 pcs - 17.53 USD다음의 수량에 대한 총 가격 1 pcs - 17.53 USD
다음의 수량에 대한 순 가격 3 pcs - 15.44 USD다음의 수량에 대한 총 가격 3 pcs - 15.44 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
QTRX-MD-16A REFLECTANCE SENSOR ARRAY | 감지기: 거리; 반사식; 2.9÷5.5VDC; 아날로그식의; Ch: 16; 125x16.5mm; MD
감지기: 거리; 반사식; 2.9÷5.5VDC; 아날로그식의; Ch: 16; 125x16.5mm; MD
제조업체 부품 번호: QTRX-MD-16A REFLECTANCE SENSOR ARRAY
제조사: POLOLU
다음의 수량에 대한 순 가격 1 pcs - 40.63 USD다음의 수량에 대한 총 가격 1 pcs - 40.63 USD
다음의 수량에 대한 순 가격 3 pcs - 35.85 USD다음의 수량에 대한 총 가격 3 pcs - 35.85 USD
4 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
VL53L3CX TIME-OF-FLIGHT MULTI-TARGET DIS | 감지기: 거리; 레이저; 2.6÷5.5VDC; I2C; 거리 범위: 0.01÷3m; IC: VL53L3CX; 해상도: 1mm
감지기: 거리; 레이저; 2.6÷5.5VDC; I2C; 거리 범위: 0.01÷3m; IC: VL53L3CX; 해상도: 1mm
제조업체 부품 번호: VL53L3CX TIME-OF-FLIGHT MULTI-TARGET DIS
제조사: POLOLU
중요한 정보: 주의! 레이저 방사선! 안전 지침을 준수하십시오. 레이저 광원을 직접 응시하지 마십시오.
다음의 수량에 대한 순 가격 1 pcs - 21.81 USD다음의 수량에 대한 총 가격 1 pcs - 21.81 USD
다음의 수량에 대한 순 가격 3 pcs - 19.32 USD다음의 수량에 대한 총 가격 3 pcs - 19.32 USD
13 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
DFR0315 | 감지기: 2D 스캐너; 레이저; 5VDC; USB-UART; 0.15÷12m; 2Hz,5.5Hz,10Hz; 360°
감지기: 2D 스캐너; 레이저; 5VDC; USB-UART; 0.15÷12m; 2Hz,5.5Hz,10Hz; 360°
제조업체 부품 번호: DFR0315
제조사: DFROBOT
중요한 정보: 주의! 레이저 방사선! 안전 지침을 준수하십시오. 레이저 광원을 직접 응시하지 마십시오.
다음의 수량에 대한 순 가격 1 set - 102.62 USD다음의 수량에 대한 총 가격 1 set - 102.62 USD
1 TME에 재고 있음
완전한 세트 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
5550 | 감지기: 거리; 반사식; 3÷5.5VDC; 숫자의; 판재 사이즈: 21.59x8.89x3.1mm; 범위: 500mm; 1개
감지기: 거리; 반사식; 3÷5.5VDC; 숫자의; 판재 사이즈: 21.59x8.89x3.1mm; 범위: 500mm; 1개
제조업체 부품 번호: 5550
제조사: POLOLU
다음의 수량에 대한 순 가격 1 pcs - 18.02 USD다음의 수량에 대한 총 가격 1 pcs - 18.02 USD
다음의 수량에 대한 순 가격 3 pcs - 15.93 USD다음의 수량에 대한 총 가격 3 pcs - 15.93 USD
5 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
표준 오퍼에 포함되지 않은 제품에 대한 요청
요청이 성공적으로 전송되었습니다. 곧 제공된 이메일 주소로 제품 구매 제안서를 보내드리겠습니다.
고객 번호
제조업체 부품 번호
제조 업체
총액
이메일주소
메시지 내용