+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

CHEMTRONICS

Chemtronics was founded in 1958 in the United States. Since the beginning, the company has dealt with the manufacturing of chemical and cleaning solutions for the industry – among others for electronic and telecommunications industries. In 1999, Chemtronics was incorporated into the ITW concern (Illinois Tool Works Inc.).
The offer of products includes, among others:

  • unsoldering strips
  • masks for wave soldering
  • cleaning and preserving products for PCB plates
  • cleaning rods and rags
  • fiber optic cleaning agents

All ITW Chemtronics products are manufactured according to the ISO9001:2000 norm.