+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

FAVIER

Favier's history dates back to the 1930s, when the company started producing wooden braiding machines. Since then, it has expanded into the production of braided sleeving and insulating tubes for a range of industries, including aeronautical, automotive, chemical, electrical, electronic, medical, metallurgical, petrochemical, railway, and shipbuilding industries.

The Favier brand uses advanced materials in the production process, characterised by high resistance to mechanical and thermal factors. In addition to silicone and glass fibre , these include, for example, silica and basalt fibres. By developing braid technology and production processes, Favier has become one of the leading European manufacturers in this field. The products of this supplier are not only widely used in industry, but also in the construction and servicing of domestic appliances.