+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 32만 명 이상의 고객

Quick Buy 즐겨찾기
카트

FIBOX

FIBOX is a private company running business activity in 10 countries with four manufacturing sites and several partners on all continents.

FIBOX offers a complete manufacturing service chain from the very design of precise elements made of plastic to ready and tested systems delivered to any place in the world. FIBOX enclosures are manufactured in a modern factory close to Helsinki, Finland and in Inchon, South Korea.

Modular enclosures made of FIBOX plastic were the first enclosures made of polycarbonate(PC) introduced in 1966 to the market. This started a new era in the development of box distribution boards. Since then, active development of products and increasing export led to the fast development of the company, which continues to this day.

A standard range of FIBOX company enclosures gives designers a selection of nearly 500 enclosures for the enclosure of electrical and electronic equipment protecting them against severe surrounding conditions.

The FIBOX enclosures are produced in accordance with the following norms: EN 60529 (IEC 529), UL 50 and UL 508. Enclosures reach the safety level of IP 67, NEMA 4X and 6, 6P.

The production of enclosures is reviewed by an independent laboratory that monitors continuously. With over 700 standard accessories FIBOX enclosures are easy and flexible to use. Standard solutions exist for panels, pivoting internal door mounting, wiring systems and fan systems.