+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 32만 명 이상의 고객

Quick Buy 즐겨찾기
카트

HALDER

Halder is a German brand with a narrow specialization: this supplier deals with the production of various types of hammers, axes as well as a broad offer of locking and fixing components. The company’s success is based on high precision in production, emphasis on tool quality as well as on designing solutions based on research and shared experiences with customers.

TME first began to offer tools from the Halder portfolio - above all, hammers. These are tools adapted for typical works: assembly, paving, tinsmithing and carpentry. This assortment also includes universal products that ideally address the needs of every household or farm, but are also suitable for professional works. Depending on the model, their heads are made of elastomer, rubber, plastic, polyamide or metal (e.g. copper). Care was taken in selecting the right material for the handle (wood, glass fiber). The product range also includes tools with limited recoil, i.e. reducing the operator's wrist fatigue. It should also be highlighted that TME’s catalog includes other Halder products, such as mallets and chocks, as well as hammer components: heads, housings, exchangeable handles. The assortment also includes axes from this manufacturer.