+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

HELU

HELU was founded in 1978 in Hemmingen near Stuttgart. In the initial phase, the brand focused primarily on the distribution of cables for various applications. In 1988, it developed its own production lines, and with time it became one of the leading German cable suppliers. The company has gained a reputation on the international market thanks to a strong emphasis on innovative products and services and full automation of logistics processes.

HELU offers a wide range of highly specialised solutions. These include standard, single-core cables, and durable, corrosion-resistant telecommunication cables. The manufacturer supplies products for virtually every branch of industry, including energy, construction, transport, and agricultural industry. HELU also manufactures high-end custom cables for use in the entertainment industry (sound system installations). It should be noted that this supplier usually offers its solutions in several versions, each with unique features, e.g., the possibility to lay cables directly in the ground, small bending radius, additional insulation, etc. HELU, as one-stop solution provider, manufactures a range of accessories and other cable-related products. These include cable glands, protection tubes, cable ties and holders, or braids - essential components for various power supply and signalling systems, as well as for the installation of cables.

With rigorous testing processes and a practical approach to customer needs, HELU is one of the leading cabling manufacturers in the TME range. HELU is a highly automated company that places great emphasis on the environmental impact of its processes, while its products are characterized by an excellent price-performance ratio. The cables of this brand have numerous certifications and meet European, US, and international standards.