+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 32만 명 이상의 고객

Quick Buy 즐겨찾기
카트

IQRF TECH

IQRF Tech s.r.o. is a technological company of Microrisc s.r.o. The company is based in the Special Economic Zone in Jičín, the Czech Republic.

The company's flagship product is the IQRF® wireless technology developed since 2004. IQRF® is a reliable, safe and unique wireless communication method operating in the Sub-GHz radio band (433-868-916MHz). It enables the transmission of small amounts of data with minimal power consumption. IQRF® can work in the POINT-POINT, STAR, and MESH topologies.

IQRF Tech also provides software for easy network creation, management and control of its key parameters. The manufacturer provides free examples of software with source codes, which customers can use for their own applications. An SDK (Software Development Kit) is also available for use on popular single board computers. The manufacturer's offer is complemented by accessories such as gateways, antennas, remote controls or controllers.

Products by IQRF Tech are an excellent starting point for creating IoT (Internet of Things) applications. They support the full autonomy of the created network and at the same time ensure interoperability with all existing communication standards, such as Wi-Fi, GSM or Ethernet. It is also important for customers that the company offers high quality technical support.

Products by IQRF Tech are applied in the following areas:

  • lighting control,
  • industrial automation,
  • measuring systems,
  • building automation,
  • Machine to Machine (M2M), Internet of Things (IoT/IIoT) and Industry 4.0 communication,
  • other control systems.