+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

KESD

KESD was set up in China and has been operating on the market since 2003. It specialises in industrial air ionisation solutions designed for production lines. The KESD products are sold in many countries, from the USA to Japan.

The products that have made their way from the KESD portfolio into the TME catalogue mainly include ionisers for electrostatic charge neutralisation. Such devices are used in the production or servicing of electronic circuits, but also in places such as printing houses, textile mills, warehouses and laboratories – not only do they reduce the risk of ESD, but also allow for safe non-contact cleaning of components and PCBs of any tarnish, dust and dirt, etc. The available products can be hung over work areas, placed on worktops or operated manually (gun-type ionisers). Moreover, KESD also offers compact ioniser modules designed for industrial automation systems – they can be integrated into production and distribution lines or connected to existing compressed air systems.