+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

KIOXIA

KIOXIA was formerly a part of Toshiba Memory Corporation. It was under this conglomerate that the world’s first NAND Flash memories were developed in KIOXIA laboratories in the 1980s. Nowadays, it is one of the leading manufacturers in the field of electronics, it also enjoys clients’ trust and is recognized as a leader of the dynamically developing SSD memory industry.

KIOXIA’s consumer products are the first to become a part of TME’s offer. These are flash drives and SD cards (HC Micro). Thanks to the profound knowledge and care for the highest standards of the production process, products of this Japanese company are distinguished by durability and they meet the expectations of even the most demanding users. Apart from basic tasks, such as data storage and archiving, KIOXIA’s rapid memories are applied in DSLR cameras, digital cameras, mobile phones, etc. These products will also work perfectly as compact memories for discrete NAS devices, often built on the basis of single-board computers (e.g. Raspberry Pi).