+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 32만 명 이상의 고객

Quick Buy 즐겨찾기
카트

KNITTER-SWITCH

Knitter-Switch has over 60 years of experience in manufacturing switches and other electromechanical components. It is a German company whose main focus is developing and manufacturing high quality switching components, using the latest findings in the fields of precision engineering, chemistry, and material science in the manufacturing process. The company’s manufacturing facilities located in Hong-Kong have been granted the international quality certificate ISO 9001.

In the TME’s catalogue, the range of Knitter-Switch products consists of, among other things, toggle switches, TACT and SNAP ACTION microswitches, which are popular solutions used in the interfaces of consumer and industrial appliances, push button switches (including vandal-resistant components). Moreover, the manufacturer offers miniature components, such as slide switches in SMD housings, encoding switches, DIP-switches – components used in controller circuits for entering initial settings. It is important to emphasise that all Knitter-Switch products are made with excellent precision and are highly durable.