+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

KOLVER

KOLVER Srl was established in 1989 and is now one of the most important manufacturers of specialist electric screwdrivers. The manufacturer has earned its reputation by developing solutions that are distinguished by reliability and precision, as well as comfort of use (low noise levels) and energy efficiency. Moreover, they are resistant to electrostatic discharge. The durability of KOLVER’s products will satisfy professionals who use power tools in their everyday work, especially those working in manufacturing plants, where electric screwdrivers are used on manufacturing lines. The high quality of the KOLVER offering is assured by the ISO 9001:2015 certificate.

In the TME catalogue, you can find not only KOLVER’s screwdrivers but also a variety of accessories and spare parts thanks to which the lifespan of the power tools offered by this Czech manufacturer can be significantly extended. KOLVER’s components, such as switches, commutator brushes, and even spare screws and springs, are available directly from the TME stock, which speeds up the service and maintenance work and allows to save money and reduce downtime.