+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

LEGRAND

LEGRAND is a leader on the market of electrical accessories, as well as an expert in the field of IT networks in residential, commercial, and industrial construction industry in countries like France, Italy, Poland, Spain, or the U.S. LEGRAND hires nearly 33,000 employees in over 30 manufacturing plants throughout the world. The company allocates up to 5% of its turnover to research and development, which has resulted in nearly 5,000 registered patents.

TME’s offer includes i.a. installation protections, relays or contactors from LEGRAND.