+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

MBS AG

Established in 1977, the German company MBS AG is one of the world leaders in manufacturing low-voltage transformers and measuring transducers. Its products are applied in machine construction, installation engineering, renewable energy, and even in the shipbuilding industry. In addition to the quality confirmed with many certificates, MBS AG prioritises its own research and development. Its efforts were awarded in 2016, when the brand was included in the list of 100 most innovative midsized companies.

TME offers MBS AG’s current transformers. The supplier’s solutions are designed for measuring currents reaching up to 1500 A. Our catalogue includes many of the manufacturer’s series of products, with a diverse range of properties, adapted for vehicles and automation systems as well as for devices applied in the power generation industry. With such a comprehensive assortment, our clients will surely find the solution they are looking for – even if the target application involves measuring high currents and offers very limited mounting space.