+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

NEXANS

The history of Nexans dates back to the 19th century. It is already since then that the company has been designing and producing cables for various applications – from precise measuring to power solutions. In over 100 years of activity, Nexans has become one of the major players on the global cabling market. The company is also a pioneer of eco-friendly production that reduces the emission of greenhouse gas by using certified, environmentally friendly materials, which are also designed for application with renewable energy sources.

The main products from Nexans offer that can be found in the TME catalogue are data cables, which are high quality multi-core, ethernet cables, intended for serial buses and installation in cable guides (automation control). They are designed with industrial applications in mind. Depending on the series, the products are characterised by their resistance to mechanical, chemical, and electromagnetic factors (shielding with the use of foil or braid), as well as their wide operating temperature range. Nexans’ products are compliant with multiple international norms, including the UL 1581 American National Standard and CSA FT1 flammability requirements.