+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

NSK

In 1914, Nippon Seiko Limited Partnership Company started its business by developing a technology for producing ball bearings. Just two years later, the company, being among the first ones in Japan, launched regular manufacturing and changed its name to NSK. In the 1960s, the company opened its first office abroad – in the state of Michigan, the USA. Since then, NSK has been continuously expanding its business and is now present on all global markets, with a total of over 200 manufacturing plants, offices and service centres. The specialist knowledge and precision in metal processing (which is NSK’s domain) are implemented to manufacture a wide range of products. These include manufacturing machine components and entire devices in the field of automation, as well as a broad offer of high-class substitutes.

The NSK products offered by TME include primarily high-class bearings. These are ball (and cone) components, made with manufacturer’s signature precision, and a selection of high-quality materials guaranteeing the long lifespan of the products.