+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

PENTEL

Pentel was founded at the end of the 1940s in Japan, and the company’s name is closely connected with the paper industry. The company has over 20 sales departments all over the world. Pentel produces reliable supplies that make the everyday office or school work easier. They guarantee not only fully comfortable writing or drawing, but abpve all safe use.

The symbol and the trademark of Pentel are soft, colourful pastels, which were invented in 1955. Moreover, Pentel created the first automatic pencil and oil-based ink marker in the world, ZEH erasers, reliable ZL36correction pens or the BK77 pen.

Manufacturer’s broad portfolio of products comprises, among others, safe, non-toxic and colourful:

  • fineliners and fountain pens,
  • pens,
  • refills,
  • markers,
  • highlighters,
  • felt-tip pens,
  • correction products,
  • pencils and leads,
  • erasers,
  • glues.

Pentel products are made from the highest quality materials, in accordance with the environmental policy (implementing the modern recycling processes and the responsible waste sorting) and respecting worker’s rights. Pentel factories operate in accordance with ISO 14001 and ISO 9001 norms.