+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

POLAM-ELTA

The history of the Polish company POLAM-ELTA dates back to 1989, when it was established as a result of the transformation of the Optoelectronics Department at Rosa Luxemburg Vacuum Tube Manufacturing Plant. Thanks to the acquisition of the experience and the manufacturing technology for light-emitting diodes, it became the only LED manufacturer in Poland. Today, POLAM-ELTA specialises in manufacturing signalling devices, indicators, and miniature light sources. The company cooperates with several universities in Poland. Thanks to that, the company’s manufacturing technologies are continuously developed, and its products are often used for scientific research – which is the best proof of their quality.

In the TME catalogue, you will find POLAM-ELTA’s LEDs with diameters of 16 mm and 20 mm, as well as LED indicators for voltages from 12 V to 230 V (assembled, with wires) available, e.g. in the IP67-rated variant. The manufacturer also offers LED-based substitutes for classic lightbulbs (e.g. BA15, E10, E14).