+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

QUICK

QUICK ELECTRONIC Co. Ltd. Was established in 1993 and since then has become one of the leading Chinese manufacturers of soldering equipment. It offers a wide range of high-quality products that are compliant with international standards (such as ISO 9001) and are much appreciated on global markets. The brand puts a lot of emphasis on eco-friendliness, so its manufacturing facilities are ISO 14001 certified.

QUICK offers a wide selection of soldering equipment. This includes soldering, desoldering and hot air stations. The company is also a supplier of equipment used in electronic service centers, as well as preheaters and solder pots intended for the repair and assembly of PCBs. Apart from this, the manufacturer provides an extensive selection of soldering tips and nozzles along with a series of fume extractors (required in environments where soldering equipment is frequently used for the assembly and disassembly of electric circuits).