+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

SANDISK

SanDisk Corporation is an American corporation that has been developing mass storage technologies since 1988. It’s one of the world leaders in the field. More than 5000 patents and multiple awards in the Thomson Reuters ranking for the most innovative companies attest to its modern approach. In 2016, SanDisk was acquired by Western Digital Corporation, one of the biggest hard disk drive producers.

SanDisk flash memory products, which enjoy consumer confidence, could not be missing from the TME catalogue. The are available as various models of flash drives and SD cards, from 16 GB to 1 TB. They are manufactured to the newest standards (USB 3.1, UHS II etc.), which, interestingly, are being developed in cooperation with the manufacturer. Due to high write and read speeds, clear declaration on dedicated products (like Raspberry Pi, GoPro), clients can be sure that they are choosing the best solution for the intended application.