+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

SANYOU

Sanyou is a Chinese company founded in 2008, which specialises in the design and manufacture of inductive and electromagnetic components. The brand operates worldwide, including in China and the USA, and employs more than 3,000 people. In addition to advanced production lines, Sanyou has its own R&D department, certified to German (VDE), US (UL) and national (CNAS) standards. Its laboratories constantly develop innovative solutions – as of today, the company can boast more than 400 patents.

Products by Sanyou available in the TME catalogue mainly include miniature electromagnetic relays and power relays. The former comprise components intended for through-hole mounting (THT) that are capable of handling currents of up to 20 A and switching mains circuits. Their coils operate at typical voltages encountered in industrial machinery, domestic appliances and similar electrotechnical equipment. Naturally, power relays offer much more extensive characteristics, and are capable of handling voltages of up to 277 V AC at currents as high as 40 A. They come in THT versions with connector leads, among others, which facilitates their connection and the manufacture of target drivers/controllers. It should be emphasised here that the Sanyou range of products has been introduced into the TME catalogue relatively recently and is constantly evolving.