+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

STABILO

The beginnings of German brand STABILO date back to 1925. It was then introduced to the market by Stabilo International GMBh, one of the manufacturers belonging to the international Schwan-Stabilo group.

STABILO is currently one of the world leaders of the stationery market, which represents German quality and consistently provides writing, drawing, colouring and highlighting supplies to its clients. The distinctive features of the office supplies by STABILO are the impressive palette of colours and the use of ground-breaking technological solutions translating into high quality and durability of the products.

STABILO was the first company on the wooden pencils market which has been certified with the FSC® certificate confirming that the majority of timber used in the production comes from environmentally-friendly and socially responsible commercial forests.

The wide range of stationery supplies from STABILO includes, among others: felt-tip pens, fountain pens, fineliners, ballpoint pens, pens and crayons.

One of the flagship products of STABILO are the BOSS ORIGINAL highlighters and Point 88 fineliners, introduced in the 1970s. STABILO BOSS ORIGINAL highlighters have been appreciated by the users for the colour palette, replaceable refills and 4-hour dry-out protection when a pen is left without a cap. High-quality Point 88 is one of the most recognizable fineliners in Europe. The product is appreciated for the production quality and the functional qualities such as: resistance to damage, non-drying tip when left without a cap and a choice of over 40 colours.