+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

VOGT

Vogt AG Verbindungstechnik was established in 1962 as a retail electromechanical company. Having experienced delayed supplies, the company decided to start processing pipes on its own, which brought new opportunities to the brand. In the 1990s, Vogt developed its business activity in the field of plastic components. Currently, the company is a renowned international supplier of components for telecommunication, automotive, electronics and household appliances.

Vogt AG’s assortment of products includes insulated and non-insulated connectors (push-on and eyelet versions) as well as cable ferrules and soldering terminals (PCB mount). Moreover, Vogt manufactures a selection of screw spacer sleeves, which are available at TME.