+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

Wakefield Thermal

Wakefield Thermal is a US-based company specialising in the manufacture of accessories for electronics. The manufacturer's portfolio includes mainly devices related to thermoregulation of components such as ICs or LEDs – these include, among others, heat sinks, pads, heat transfer pads, fans or Peltier modules and heat pipes. Their manufacturer is a brand which has been operating on the American and world market for nearly 70 years. Today, it cooperates with companies from a variety of industries – including arms and transportation industry – but also small businesses that have found a source of solid and proven solutions in Wakefield Thermal.

Thermoregulation, on which Wakefield Thermal focuses, is a key issue for all electronic devices, especially for converters, stabilizers and high-power signal-generating circuits (e.g. controllers), as well as microcontrollers and processors with a high computing power. These are components of devices and machines applied in the field of renewable energy, IT, telecommunications, as well as LED lighting and the medical industry.

Solutions by Wakefield Thermal are an important part of TME’s offer and mainly include heat sinks, their accessories and DC fans. These products are tailored to different needs (e.g. heat sinks for TO-218 or TO-220 packages), universal solutions (e.g. heat pipes), made of high-quality materials.