+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

ZETTLER

ZETTLER is one of the best-known manufacturers of relays in the world. With over 100 years of experience, it has worked its way up to the top, focusing on the development of the semiconductor technology. In the following steps, it entered the market of switches, thermostats, transformers, and even TFT/LCD displays. ZETTLER components are commonly used in household appliances, audio/video equipment, and in complex industrial controllers.

In the TME catalogue, ZETTLER is primarily represented by electromagnetic relays. It is a very wide choice of products with a varied scope of parameters, designed for different types of applications – rated coil voltages reach up to 3–240 V DC, and the maximum contact current can reach up to even 150 A in the case of some models. Various versions are available, including bistable, monostable – miniature and subminiature – signal, interface, automotive and power relays. Apart from relays, the TME catalogue also includes other products by ZETTLER, such as encapsulated, compact transformers.