+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

Test probes – types and application

게시 날짜: 03-08-2021 업데이트 날짜: 10-04-2026 🕒 51 읽기 시간

Production of electronic circuits on a mass scale requires far-reaching automation. This applies to the manufacture of PCBs, the placement of components, as well as their soldering. However, even the most efficient production process can be slowed down at the final quality control stage. That's why advanced ICT (In-Circuit Tests) solutions, which verify a circuit and its parameters through an automated series of measurements, are being used more and more on production lines. Obviously, this type of inspection has been performed for decades – but the increasing miniaturisation of electronics requires ever more precise probing of PCBs and wire harnesses. In the era of communication circuits operating at enormous frequencies, the measurements themselves must also be more accurate, while the general use of digital circuits has irreversibly changed ICT methodologies. Today we often encounter the abbreviation FCT (functional testing), which refers to the detailed verification of a circuit's operation already in the final production stage, by powering it up and simulating its operation in the finished device.

Electronic circuit testers are made of a lot of components – holders, controllers, measuring circuits, sensors. They are programmable and configurable devices. They also contain one essential operating element: test probes. These are precision, spring-loaded probes designed to make good, but short-lived, contact with circuit elements – primarily the leads of passive components and ICs and areas on a PCB. Besides making measurements and checking the continuity of paths, they are also used for other purposes. They can penetrate connectors and allow contact connection testing without exploiting the socket or plug housing. They are also used in digital electronics, where they are applied, among other things, to program microcontrollers using the ISP (In-System Programming) technique and to carry out tests by communicating with the systems installed in the circuit (e.g. by means of a serial port or the CAN bus in the automotive sector). Specialised contact probes are used in the manufacture of batteries, or rather cells and packs, which need to be charged to the optimum level for storage and transport before being stored. An important area of application for contact probes is in electronic services, where automated circuit testing can speed up the process of fault detection and rectification.

Contact probes – the basic parameters

The first difference between the contact probes can be seen at a first glance. This is the shape of the tip (head). We will discuss the purpose of individual heads later in this text. We will first focus on the electrical and mechanical parameters, which should be taken into account in the context of the type of test performed.

As probes are subject to constant use and pressed against PCB components over and over again, they are subject to wear and contamination. Nowadays, with the electronics industry commonly turning to lead-free binders (harder and requiring more chemically aggressive fluxes), the hardness and coating of the contact probes plays a particularly important role. Therefore, we often encounter steel probes and probes made of beryllium copper (CuBe), an alloy characterised by high durability and electrical conductivity comparable to pure copper. To protect the tips from corrosive influences, the probes are usually coated with gold or nickel – in this way they retain their durability even in frequent contact with fluxes and their solvents.

It is important to pay attention to the fact that a simple zero-one continuity test can be performed with probes of relatively high resistance. However, a detailed circuit inspection (or calibration) will rely on a precise measurement whichrequires connections with the lowest possible resistance. Therefore, the nominal resistance will be found in the characteristics of all contact probes. Here, a related factor is the lateral spring deflection – as only the pressure according to the manufacturer's recommendations guarantees obtaining a connection with the specified resistance (working deflection will occur after applying a power determined by a separate parameter). Please beware: (1) the spring compression should not exceed the maximum stroke (in such a situation the probe will not be cushioned); (2) the pressure force is transferred to the components of the tested circuit – an incorrectly selected probe may damage components, paths, etc.

The last important parameter isacceptable working temperature – because automated tests are sometimes carried out between circuit production steps or shortly after the reflow soldering process. In other words, there are situations where the probe is in contact with high temperature components. This also applies to the conditions of so-called stress tests and environmental tests, when the behaviour of a circuit subjected to maximum loads or under extreme thermal conditions is examined.

When selecting probes for testing circuits with a high density of components, another parameter will be important – the minimum pitch in which a given probe can operate.

Application and types of test probes

Electronic circuits are most often probed:

  • in specially designated areas (test pads), which in precision electronics are often covered with gold plating (Fig. 1b, 1c, 1d);
  • on connections between PCB and leads of components (Fig. 1e);
  • VIA points (Fig. 1a), i.e. sleeves connecting PCB layers (most often we are dealing with double-sided boards, but in case of computer or mobile phone motherboards, for example, circuits consist of more layers);
  • on contacts of pin connectors and similar connectors (Fig. 1f).

Depending on the point to be tested, as well as the need (or lack thereof) to penetrate deposit, oxidised solder or flux residues, a probe with the proper head shape should be selected to perform the test. So let's take a look at what functions are provided for each solution.

Fig. 1. Test pads of electronic circuits.

Cylindrical or hemispherical probes

 
 
Probes equipped with cylindrical, flat (Figs. 2, 3) or hemispherical (Figs. 4, 5) tips are a safe tool for probing test pads** (especially those gold-plated and cleaned). Hemispherical tips can also be successfully used for measurements made on solder leads or the leads themselves. The overriding feature of such tips is non-invasiveness.

Rounded tip prevents scratching the tested components.

TME also offersprobes with a cylindrical tip with a tapered flute (Fig. 6, 7). This shape facilitates tests carried out on male pin connectors or in place of assembly of THT elements. The wide opening allows to "grab" leads even if they are bent or placed imprecisely. Specialists point out that the tapered flute can quickly become contaminated – if the probe is operated in sub-optimal conditions or in testing services for used and dirty equipment. Nonetheless, it is one of the most popular solutions for the verification of through-hole circuits. Similar properties are found in radial milled heads (Fig. 8) – while also being compatible with flat and convex test points.

Fig. 2

Symbol: Operational spring compression: Diameter: Imax: Rmax:
IT125-P10 6.35mm no data 10A 9mΩ
TK0030N.F150S120A 2mm no data 3A 15mΩ
TK0045N.F150C200A 5.1mm no data 3A 10mΩ
TK0050N.F254C120A 5.1mm no data 3A 15mΩ
TK090N.10100S130N 3.6mm no data 3A 40mΩ
TK32N.10200S170A 4.2mm 2mm 3A 10mΩ
TK32N.10250S170A 4.2mm 2.5mm 3A 10mΩ
TK32SCR.10150C150A 4mm 1.5mm 5A 10mΩ
TK32SCR.10200S150A 4mm 2mm 5A 10mΩ
TK36L.10140S170A 5mm 1.4mm 3A 10mΩ
TK36L.10250S170A 5mm 2.5mm 3A 10mΩ
TK36N.10180S170A 4.5mm 1.8mm 5A 10mΩ
TK36SCR.10140S300A 4mm 1.4mm 5A 10mΩ
TK37N.10230M300A 4.5mm 2.3mm 3A 10mΩ
TK37N.10400M300A 4.5mm 4mm 3A 10mΩ
TK37N.10650M300A 4.5mm 6.5mm 3A 10mΩ

Fig. 3

Symbol: Operational spring compression: Diameter: Imax: Rmax:
TK0030N.C066S120A 2mm no data 3A 15mΩ
TK0045N.C104C200A 5.1mm no data 3A 10mΩ
TK0050N.C173C120A 5.1mm no data 3A 15mΩ
Fig. 4
Symbol: Operational spring compression: Diameter: Imax: Rmax:
50.105.25.20 3.4mm 2.5mm 4A, 5.5A 20mΩ
60.05.33.30 4mm 3.3mm 4A, 5A 20mΩ
TK0030N.D102S120A 2mm no data 3A 15mΩ
TK0045N.D127C200A 5.1mm no data 3A 10mΩ
TK0050N.D254C120A 5.1mm no data 3A 15mΩ
TK090N.05100S130N 3.6mm no data 3A 40mΩ
TK100N.05135S280N 3.4mm no data 3A 55mΩ
TK100N.05190S280N 3.4mm no data 3A 55mΩ
TK32N.05065S170N 4.2mm 1.6mm 3A 10mΩ
TK32N.05130S170A 4.2mm 1.3mm 3A 10mΩ
TK32N.05200S170A 4.2mm 2mm 3A 10mΩ
TK32SCR.05130S150A 4mm 1.3mm 5A 10mΩ
TK32SCR.05200S150A 4mm 2mm 5A 10mΩ
TK35N.05130S170A 6.4mm 1.3mm 3A 10mΩ
TK35N.05200S170A 6.4mm 2mm 3A 10mΩ
TK36L.05250S170A 5mm 2.5mm 3A 10mΩ
TK36N.05250S170A 4.5mm 2.5mm 5A 10mΩ
TK36SCR.05230C300A 4mm 2.3mm 10A 10mΩ
TK36SCR.05300C300A 4mm 3mm 10A 10mΩ
TK37N.05230M300A 4.5mm 2.3mm 3A 10mΩ
Fig. 5

Symbol: Operational spring compression: Diameter: Imax: Rmax:
150.105.25.20 3.4mm 2.5mm 4A, 5.5A 20mΩ
30.05.13.15 3.3mm 1.3mm 3A, 4A 20mΩ
31.05.13.15 3.3mm 1.3mm 3A, 4A 20mΩ
40.05.15.15 5.3mm 1.5mm 3A, 4A 20mΩ
40.08.13.15 5.3mm 1.3mm 3A, 4A 20mΩ
TK0030N.J066S120A 2mm no data 3A 15mΩ
TK0045N.J104C200A 5.1mm no data 3A 10mΩ
TK0050N.J173C120A 5.1mm no data 3A 15mΩ
TK0064B.J.2.60.57 2.75mm no data 3A 25mΩ

Fig. 6

Symbol: Operational spring compression: Diameter: Imax: Rmax:
100-PRG2522S 4.24mm no data 12A 15mΩ
IT100-P22 6.35mm no data 6.5A 13mΩ
IT125-P22 6.35mm no data 10A 9mΩ
TK0030N.A127S120A 2mm no data 3A 15mΩ
TK0045N.A150C200A 5.1mm no data 3A 10mΩ
TK0050N.A254C120A 5.1mm no data 3A 15mΩ
TK32N.09200S170A 4.2mm 2mm 3A 10mΩ
TK32SCR.09130C150A 4mm 1.3mm 5A 10mΩ
TK32SCR.09200S150A 4mm 2mm 5A 10mΩ
TK36L.09250S170A 5mm 2.5mm 3A 10mΩ
TK36L.09400S170A 5mm 4mm 3A 10mΩ
TK36N.09250S170A 4.5mm 2.5mm 5A 10mΩ
TK36N.09400S170A 4.5mm 4mm 5A 10mΩ
TK36SCR.09230C300A 4mm 2.3mm 10A 10mΩ
TK37N.09230M300A 4.5mm 2.3mm 3A 10mΩ
TK37N.09400M300A 4.5mm 4mm 3A 10mΩ
Fig. 7

Symbol: Operational spring compression: Diameter: Imax: Rmax:
TK0030N.G066S120A 2mm no data 3A 15mΩ
TK0045N.G104C200A 5.1mm no data 3A 10mΩ
TK0050N.G173C120A 5.1mm no data 3A 15mΩ
Fig. 8
Symbol: Operational spring compression: Diameter: Imax: Rmax:
TK090N.16100S130N 3.6mm no data 3A 40mΩ
TK100N.16135S280N 3.4mm no data 3A 55mΩ
TK100N.16190S280N 3.4mm no data 3A 55mΩ

Multi-purpose probes

 
The tips described above have one flaw that can prove critical in manufacturing processes using lead-free solder. Their design makes it difficult for deposit and flux residues to penetrate. As an alternative, cylindrical probes, the top of which has been milled to produce a matrix of pyramids, are available. Not only can such probes be used to connect to most test points (test pads, THT leads, etc.), they also penetrate the top layer of binder (e.g. oxidised), which reduces the risk of test result falsification.

Numerous vertices facilitate contact with both flat and vertical elements.

Fig. 9

Symbol: Operational spring compression: Diameter: Imax: Rmax:
IT125-P10 6.35mm no data 10A 9mΩ
TK0030N.F150S120A 2mm no data 3A 15mΩ
TK0045N.F150C200A 5.1mm no data 3A 10mΩ
TK0050N.F254C120A 5.1mm no data 3A 15mΩ
TK090N.10100S130N 3.6mm no data 3A 40mΩ
TK32N.10200S170A 4.2mm 2mm 3A 10mΩ
TK32N.10250S170A 4.2mm 2.5mm 3A 10mΩ
TK32SCR.10150C150A 4mm 1.5mm 5A 10mΩ
TK32SCR.10200S150A 4mm 2mm 5A 10mΩ
TK36L.10140S170A 5mm 1.4mm 3A 10mΩ
TK36L.10250S170A 5mm 2.5mm 3A 10mΩ
TK36N.10180S170A 4.5mm 1.8mm 5A 10mΩ
TK36SCR.10140S300A 4mm 1.4mm 5A 10mΩ
TK37N.10230M300A 4.5mm 2.3mm 3A 10mΩ
TK37N.10400M300A 4.5mm 4mm 3A 10mΩ
TK37N.10650M300A 4.5mm 6.5mm 3A 10mΩ

Fig. 10

Symbol: Operational spring compression: Diameter: Imax: Rmax:
TK0030N.C066S120A 2mm no data 3A 15mΩ
TK0045N.C104C200A 5.1mm no data 3A 10mΩ
TK0050N.C173C120A 5.1mm no data 3A 15mΩ

Fig. 11

Symbol: Operational spring compression: Diameter: Imax: Rmax:
IT100-P74 6.35mm no data 6.5A 13mΩ

Conical tips

Conical tips are the oldest and still the most widely used solution. It is important to bear in mind that they have their limitations and are a diverse product group.

The cone-shaped tips (Fig. 12, 13, 14) can be used for almost all types of tests, although they require precise positioning. Even small variations in PCB size will quickly lead to a series of incorrect measurements. The 60° and 90° bevelled ends are mainly used for testing VIA points and female connectors. Before application soldermasks can also be used to create temporary connections to a single circuit path. Again it should be noted that for bushings and connectors where the surface may be contaminated in some way the milled/fluted types (Fig. 15, 16, 17) are the best option as their edges facilitate penetration.

Precise cone, i.e. for testing of hollowed components.

The best deposit penetration in this product group is ensured by bevelled probes with an angle of 30° or even 15°. These include TEKON probes with heads 13 and 14 as well as the sharp probe 44.118.10.15 from FIXTEST (Fig. 18). These kind of probes are not recommended for testing VIA points filled with solder, because they can damage the connection between PCB layers.

A special case of contact probes with a conical tip are those with a bevelled tip (Fig. 19). Their shape allows connections to be made to many types of test points, they are the most reliable method for testing sockets, and they offer a relatively large contact area and therefore: low resistance and higher current capability.

Fig. 12

Symbol: Operational spring compression: Diameter: Imax: Rmax:
TK0030N.E127S120A 2mm no data 3A 15mΩ
TK0045N.E150C200A 5,1mm no data 3A 10mΩ
TK0050N.E254C120A 5,1mm no data 3A 15mΩ
TK090N.06100S130N 3,6mm no data 3A 40mΩ
TK100N.06190S280N 3,4mm no data 3A 55mΩ
TK32N.06200S170A 4,2mm 2mm 3A 10mΩ
TK37N.06230M300A 4,5mm 2,3mm 3A 10mΩ
TK37N.06400M300A 4,5mm 4mm 3A 10mΩ

Fig. 13

Symbol: Operational spring compression: Diameter: Imax: Rmax:
150.102.23.20 3.4mm 2.3mm 4A, 5.5A 20mΩ
154.102.23.20 3.8mm 2.3mm 4A, 5.5A 20mΩ
30.102.13.15 3.3mm 1.3mm 3A, 4A 20mΩ
31.102.13.15 3.3mm 1.3mm 3A, 4A 20mΩ
40.102.13.15 5.3mm 1.3mm 3A, 4A 20mΩ
41.102.13.15 5.3mm 1.3mm 3A, 4A 20mΩ
50.102.23.20 3.4mm 2.3mm 4A, 5.5A 20mΩ
IT075-P41 4.24mm no data 6A 2.5mΩ
IT125-P41 6.35mm no data 10A 9mΩ
TK0030N.B066S120A 2mm no data 3A 15mΩ
TK0045N.B104C200A 5.1mm no data 3A 10mΩ
TK0050N.B173C120A 5.1mm no data 3A 15mΩ
TK090N.13100S130N 3.6mm no data 3A 40mΩ
TK32N.13130S170A 4.2mm 1.3mm 3A 10mΩ
TK32SCR.13130S150A 4mm 1.3mm 5A 10mΩ
TK35N.12080S170R 6.4mm 0.8mm 3A 10mΩ
TK35N.13130S170R 6.4mm 1.3mm 3A 10mΩ
TK36L.13180S170A 5mm 1.8mm 3A 10mΩ

Fig. 14

Symbol: Operational spring compression: Diameter: Imax: Rmax:
71.102.07.30 4mm 0.7mm 3A, 4A 25mΩ
TK36N.14180S170A 4.5mm 1.8mm 5A 10mΩ

Fig. 15

Symbol: Operational spring compression: Diameter: Imax: Rmax:
TK0030N.T127S120A 2mm no data 3A 15mΩ
TK0045N.T104C200A 5.1mm no data 3A 10mΩ
TK32N.08200S170R 4.2mm 2mm 3A 10mΩ
TK32SCR.08130S150A 4mm 1.3mm 5A 10mΩ
TK32SCR.08200S150R 4mm 2mm 5A 10mΩ
TK35N.08200S170R 6.4mm 2mm 3A 10mΩ
TK36L.08250S170A 5mm 2.5mm 3A 10mΩ
TK36N.08250C170A 4.5mm 2.5mm 10A 10mΩ
TK36N.08300S170A 4.5mm 3mm 5A 10mΩ
TK36SCR.08230C300A 4mm 2.3mm 10A 10mΩ
TK37N.08230M300A 4.5mm 2.3mm 3A 10mΩ

Fig. 16

Symbol: Operational spring compression: Diameter: Imax: Rmax:
TK0030N.K127S120A 2mm no data 3A 15mΩ
TK0050N.K254C120A 5.1mm no data 3A 15mΩ

Fig. 17

Symbol: Operational spring compression: Diameter: Imax: Rmax:
TK0030N.LM127S120A 2mm no data 3A 15mΩ
TK0045N.LM150C200A 5.1mm no data 3A 10mΩ
TK090N.04100S130N 3.6mm no data 3A 40mΩ
TK100N.04190S280N 3.4mm no data 3A 55mΩ
TK100N.04250S280N 3.4mm no data 3A 55mΩ
TK100N.04350S280N 3.4mm no data 3A 55mΩ
TK32N.04200S170R 4.2mm 0.65mm 3A 10mΩ
TK35N.04200S170R 6.4mm 2mm 3A 10mΩ

Fig. 18

Symbol: Operational spring compression: Diameter: Imax: Rmax:
44.118.10.15 7mm 1mm 3A, 4A 20mΩ

Fig. 19

Symbol: Operational spring compression: Diameter: Imax: Rmax:
TK36L.11180S170A 5mm 1,8mm 3A 10mΩ
TK36N.11180S170N 4,5mm 1,8mm 5A 10mΩ

Crown-milled probes

 
It can be said thatcrown-milled probes (usually with four vertices) combine the benefits of all the solutions presented above. Although not designed for testing VIA points and female connectors, they offer: excellent penetration of coating and deposits; their numerous sharp edges make it difficult for contaminants to adhere (self-cleaning effect); surrounding the central point of the head with vertices makes it easier for the probe to contact the leads of THT components even in the case of minor assembly imperfections (bending, displacement), and focuses the probe on convex test pads.

TME offers probes with a soft (shallow, Fig. 20, 21) and sharp (Fig. 22, 23) crown tip, as well as a three-point variant (Fig. 24).

Fig. 20

Symbol: Operational spring compression: Diameter: Imax: Rmax:
154.105.25.20 3.8mm 2.5mm 4A, 5.5A 20mΩ
31.06.13.15 3.3mm 1.3mm 3A, 4A 20mΩ
TK0045N.W127C200A 5.1mm no data 3A 10mΩ
TK100N.02135S280N 3.4mm no data 3A 55mΩ
TK100N.02190S280N 3.4mm no data 3A 55mΩ
TK32N.02130S170R 4.2mm no data 3A 10mΩ
TK35N.02130S170R 6.4mm 1.3mm 3A 10mΩ
TK36L.02250S170A 5mm 2.5mm 3A 10mΩ
TK36L.02400S170A 5mm 4mm 3A 10mΩ
TK36N.02250S170A 4.5mm 2.5mm 5A 10mΩ
TK36SCR.02300S300A 4mm 3mm 5A 10mΩ

Fig. 21

Symbol: Operational spring compression: Diameter: Imax: Rmax:
30.06.13.15 3.3mm 1.3mm 3A, 4A 20mΩ
44.46.10.15 7mm 1mm 3A, 4A 20mΩ
50.06.25.20 3.4mm 2.5mm 4A, 5.5A 20mΩ
TK0030N.U030S120A 2mm no data 3A 15mΩ
TK0045N.U030C200A 5.1mm no data 3A 10mΩ

Fig. 22

Symbol: Operational spring compression: Diameter: Imax: Rmax:
150.06.25.20 3.4mm 2.5mm 4A, 5.5A 20mΩ
154.06.25.20 3.8mm 2.5mm 4A, 5.5A 20mΩ
71.106.13.30 4mm 1.3mm 3A, 4A 25mΩ
TK0030N.V150S120A 2mm no data 3A 15mΩ
TK0045N.V127C200A 5.1mm no data 3A 10mΩ
TK100N.03135S280N 3.4mm no data 3A 55mΩ
TK100N.03190S280N 3.4mm no data 3A 55mΩ
TK32N.03130S170R 4.2mm no data 3A 10mΩ
TK35N.03200S170R 6.4mm 2mm 3A 10mΩ

Fig. 23

Symbol: Operational spring compression: Diameter: Imax: Rmax:
IT075-P84 4.24mm no data 6A 2.5mΩ
IT100-P84 6.35mm no data 6.5A 13mΩ

Fig. 24

Symbol: Operational spring compression: Diameter: Imax: Rmax:
TK0045N.X150C200A 5.1mm no data 3A 10mΩ

Special purpose probes

In addition to probes for basic electrical testing, TME's range also includes specialised probes for precision measurement, LED testing and (rechargeable) battery handling.

Automated four-wire sensing

Four point/four-wire sensing involves applying four probes to a section of a circuit. The outer pair allows current to flow through the component under test, while the inner pair is used to measure the potential difference at the input and output of the component. With the current and voltage drop data, the meter determines the resistance of the probed object with high precision. Unlike a two-point sensing, the result will not be biased by the resistance of the probing leads – which is why this technique is most commonly used to test low resistances as part of testing and calibration of precision electronics (e.g. measuring devices). This method is often called Kelvin (or Kelvin) sensing/system .

To carry out four-wire sensing, a special type of contact probes is needed, each of which is equipped with two independent contacts. The elements are adapted to perform measurements on connectors and test points especially designed for this purpose. The gold plating and the material ensure repeatability and low connection resistance – even with a large number and high frequency of connection and disconnection cycles..

Probes for four-point sensing

LED testing

LED testing under mass production conditions is based on (1) electrical measurements and (2) applying power and verifying that the light emitted by the LED has the correct brightness and colour. Functionality testing also verifies that the indicators are properly communicating the status of the device. To verify the operation of the diode, special contact probes are applied to the LED and the emitted light is transmitted through an optical fibre. Further measurements are taken by a sensor placed at the other end of the optical fibre (usually measuring both the intensity and wavelength of radiation). The fibre-optic tip attached to the probe is usually located in a groove that restricts the inflow of external light, so that the test does not need to be carried out in darkness.

At TME we offer a selection of TEKON brand LED contact probes with diameters from 1.1mm to 5mm. This range coincides with the most popular sizes of light emitting diodes – from SMD components to standard THT controls.

Probes for LED testing

Battery probes

Another specific type of contact probes are items designed to create temporary connections to power source terminals. These types of probes are used when testing common consumer batteries (AA, AAA, etc.) as well as rechargeable batteries. Since all cells have an optimum degree of charge in which they should be stored, probes adapted to battery terminals are also used in the process of pre-charging batteries (in the last stage of production), which allows their safe storage and transport.

The large surface area and spring compression force guarantee a good attachment to the terminal.

Battery probe tips are usually cylindrical or hemispherical in shape. Since the size of power sources is strictly defined by international standards, battery probes are characterised by a low spring compression.

Symbol: Operational spring compression: Diameter: Imax: Rmax:
365.35.40.40 2.7mm 4mm 3A 30mΩ
365B.35.40.40 2.7mm 4mm 15A 30mΩ
FK-441 1.52mm 0.75mm 3A 100mΩ
FK-586 1.33mm 1.02mm 1A 30mΩ
FK-606B 1.33mm 1.02mm 3A 30mΩ
FK-691 1mm 1.3mm 5A 30mΩ
FK-714 1mm 1.3mm 5A 15mΩ
IT-5303 no data no data 3A 20mΩ
TK0064B.J.2.60.57 2.75mm no data 3A 25mΩ
TK53B.0.5.1.30.200 1mm no data 1.5A 10mΩ
TK54B.0.5.1.30.200 1.5mm no data 1.5A 10mΩ

Transfer Multisort Elektronik (TME)은 전자 부품, 전기 기술 부품, 작업장 장비 및 산업 자동화의 세계 최대 글로벌 유통업체 중 하나입니다. 카탈로그에는 1,300개 주요 제조업체의 1,500,000개 이상의 제품이 포함되어 있습니다. Łódź와 Rzgów (폴란드)에 있는 TME의 현대적인 물류 센터는 총 면적이 40,000 m² 이상이며 매일 약 6,000개의 패키지를 150개국 이상의 고객에게 발송합니다.

TME는 또한 TME Education 프로젝트를 통해 젊은 엔지니어와 전자공학 애호가들의 지식과 기술 개발에 투자하고 있으며, TechMasterEvent 시리즈를 조직하여 혁신과 경험 교류를 촉진하면서 기술 커뮤니티를 지원합니다。

또 읽기