+1500000 개 이상의 제품 제공
하루에 7000개의 패키지
150개국에서 28만 명 이상의 고객
게시 날짜: 29-07-2022 업데이트 날짜: 10-04-2026 🕒 3 읽기 시간
The acronym CMI&A stands for Control Measuring Instruments and Automation. It is used to describe systems that monitor all processes and, if needed, control them. Until recently, this was only important in industrial facilities and during production processes. However, now, such systems are also installed in modern housing, where their task is to control electrical energy, heat supply, sometimes also the quality of air and comfort in rooms. The system which manages temperature, ventilation, and sometimes, even air ionization or cleaning options, is called HVAC (Heating, Ventilation, Air Conditioning). It is very important in modern buildings where it is not possible to open windows.
The full version of what the acronym stands for alone gives us a picture of what this system is and what it comprises. A CMI&A system includes: sensors, gauges, recorders, transducers and other similar devices whose task is to measure the status of processes in real time, conditions in a room, consumption of various utilities, and also test any needed parameter which is important for the owner of the building or a production or treatment process. A wide range of sensors and components that are necessary for this type of a system is available from TME. Apart from measuring, such systems are able to control and also change the settings, i.e. open and close valves, switch between the programme modes, etc. Most of these tasks are automatic, and that is why automation is an important part of these systems – when controlling work processes, CMI&A systems usually use a controller which collects measured data, processes it and then sends appropriate orders to the working elements.
CMI&A equipment is usually installed in the control cabinet. These types of cabinets are most often made from prefabricated materials, as ordered by the client, in harmony with the design which precisely determines what the whole system is meant to look like. These types of CMI&A projects are usually created for industrial entities by a team of engineers who know a given industry very well and are able to foresee the required CMI&A devices, CMI&A circuits, a proper set of controllers and sometimes even order special software for this particular project and branch of industry. The programme menu which the users will use should meet all the requirements regarding the parameters and ensure a good insight into the controlling of all industrial processes in real time.
The rules of operating the CMI&A systems must be compatible with the manufacturer’s O&MM and with the Network Transmission Code (NTC), which are subject to approval of the person in charge of the system, especially for those power devices where special qualifications are needed. We need to remember that in this case, control and measurement procedures are performed on live devices and are treated as work performed in conditions posing a particular threat to human health and life. They must be done in pairs. Individuals who perform such works must hold special qualifications and skills and also a valid qualification certificate which authorises them to perform such work. The other person must be trained in first aid or hold a valid qualifications certificate.
If these are your first steps in the world of electronics and you are building your first circuits, Tech Master Event is the portal you are looking for. On the platform, you can post your own projects and look for inspiration in the works of other users.
Tech Master Event is also a hub in which you will find many competitions for your electronic engineers from all over the world.
Transfer Multisort Elektronik (TME)은 전자 부품, 전기 기술 부품, 작업장 장비 및 산업 자동화의 세계 최대 글로벌 유통업체 중 하나입니다. 카탈로그에는 1,300개 주요 제조업체의 1,500,000개 이상의 제품이 포함되어 있습니다. Łódź와 Rzgów (폴란드)에 있는 TME의 현대적인 물류 센터는 총 면적이 40,000 m² 이상이며 매일 약 6,000개의 패키지를 150개국 이상의 고객에게 발송합니다.
TME는 또한 TME Education 프로젝트를 통해 젊은 엔지니어와 전자공학 애호가들의 지식과 기술 개발에 투자하고 있으며, TechMasterEvent 시리즈를 조직하여 혁신과 경험 교류를 촉진하면서 기술 커뮤니티를 지원합니다。