+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
4.a. Shipping costs are incurred by the Customer, unless it is agreed otherwise upon a separate agreement made between the Customer and TME.
4.b. The amount of shipping costs depends on a package’s weight, its dimensions, country of destination, and a selected carrier/forwarder.
4.c. Shipping costs are added to the order and invoiced with the first shipment containing the goods from a given order. On a Customer’s request, combining additionally ordered goods with the second or any subsequent shipments containing the goods from a given order means that such shipment including additionally ordered goods will be treated as a new order and the shipping costs will be added to it. If a package weight exceeds the lump sum for a given country (or such a lump sum has not been established), then the shipping costs are calculated by the TME Export Department.
4.d. Terms of deliveries are approximate terms, unless the Customer agreed with TME the delivery term based on a separate agreement.
4.e. Term of delivery is specified in the ISO 8601 standard.
4.f. Costs and delivery times chart can be found on the www.tme.eu site in the "How to buy" section.
4.g. TME selects a forwarder/carrier, unless it has been agreed otherwise in a separate agreement between the Customer and TME. The Customer agrees that the carrier may leave the package at the delivery address without the addressee having to confirm its receipt, in accordance with the carrier’s delivery policy.
4.h. The collection of goods from TME at 41 Ustronna str. is possible only after individual arrangements to that end are made by the Customer and TME.