+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
This is a feature that allows you to load products from your Favorites.
Simply select the folder from which you want to download the products and confirm your choice by clicking the “Load”. button.
Then, define how many times a given folder is to be added to Quick Buy. This option is useful if a specific folder is to be ordered repeatedly. Thanks to this, you won’t have to load it to Quick Buy several times.
After entering the list of products, a summary appears on the screen, in which you can check the accuracy of product lines entered.
In the case of a mistake related to entering the product, a message is displayed indicating the type of error. You have to correct the wrong line and then accept the changes with "Enter" or by clicking the floppy disk icon at the end of the line.