PROXXON
Proxxon is manufacturer known for power tools and hand tools for precision applications. The range of power tools includes, among other things, polishers, miniature drills, jigsaws and sanders. They are powered with 12V and 220V, and their weight starts from as little as 100g. Among hand tools, it is worth pointing out wrenches and torque screwdrivers. Thanks to the use of CrV31 and CrV3 steel with increased content of carbon compounds in the manufacturing process, the key components of these tools are sturdier and more durable. Because of their expertise, the engineers at Proxxon also ensure the functionality and manufacturing accuracy of the tools in their offer.
The company operates in over 80 countries, and micro tools by Proxxon are used by professionals from such sectors as electronics, optics, jewellery, watchmaking, or prosthetics. They are also often used by enthusiasts of scale models.