+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Do AAA and AA batteries differ only in size?

No, AAA and AA Batteries are not only different in size - they also have different capacities, current outputs and typical applications. Both types deliver the same voltage, but are not interchangeable and are designed for different devices.

Voltage versus capacity

Both AA and AAA Batteries have a nominal voltage of 1.5 V (in the alkaline version) or 1.2 V (in the rechargeable version, e.g. NiMH). This means that they can power similar electronic systems, but differ in the amount of energy they are able to deliver. Batteries AA (approx. 14.5 mm diameter, 50.5 mm length) have a much larger volume than AAA (approx. 10.5 mm diameter, 44.5 mm length), which translates into a larger capacity. A typical AA battery can have between 2,000 and 3,000 mAh, while AAAs typically reach 800-1200 mAh, depending on the type and manufacturer. This means that an AA battery will last much longer with the same load.

Differences in applications

Due to their characteristics, AA batteries are the battery of choice for devices with higher power consumption, such as Torches, electronic toys, console controllers and photographic equipment. In contrast, AA Batteries are used in compact and energy-efficient devices, e.g. remote controls, wireless mice, clocks and remote controls. In devices designed for low power consumption, a larger capacity AA battery could be an inefficient design solution - it would take up more space and the energy savings would be small.

Can AA and AAA batteries be used interchangeably?

No, although the voltage is the same, AA and AAA batteries have different dimensions and do not mechanically fit into the same sockets. Adapters exist that allow you to use AAA cells in devices that require AA, but this involves a loss of capacity and a shorter operating time. In summary, the difference between AA and AAA is not only a matter of size, but also capacity and application. Choosing the right type depends on the requirements of the device and its design.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO