+1500000 sản phẩm cung cấp

7000 đơn hàng mỗi ngày

300000 khách hàng đến từ 150 quốc gia

Quick Buy Mục ưa thích
Giỏ hàng

MESTO

MESTO is a German company with a strong family tradition. It all began in 1919 in Freiburg, where two brothers, Karl and Ernst Stockburger, founded their workshop. With time, their business has expanded tremendously, and today it is an advanced company with an extensive manufacture and development facilities, managed by Bernd Stockburger, the grandson of the company’s founders. MESTO is a leading producer of high pressure sprayers, which can be used for the application and dosing of various substances, from fertilizers to impregnating agents and preservatives. Such tools are used in a wide range of industries, such as automotive, horticulture, agriculture, gardening, forestry, as well as cleaning works. They are also often used for applying coolants during industrial cutting and boring operations.

There are several groups of MESTO products available in the TME catalogue which should be highlighted. First, there are classic trigger and pressure sprayers equipped with jet nozzles and adjustable atomizers. Selected models feature a hand pump which helps to obtain higher pressure in the tank. MESTO also provides bulkier versions of such devices, equipped with shoulder straps to carry the sprayer like a backpack – this solution is often used in gardening. The most advanced sprayer models can be connected to an external compressed air source, and their nozzles are fitted on an elongated spray pistol, which facilitates distribution of liquids in high or otherwise inaccessible places. Most of these products are designed to handle a diverse range of chemicals, such as: alcohols, acids/alkalis, oils and paraffin. Depending on the size, tanks can hold from one to over a dozen litres.